imx8qxp uuu烧录问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp uuu烧录问题

3,269 Views
475143463
Contributor III

imx8qxp-mek开发板,yocto编译的4.14.98的内核和2018.03的BootLoader。

并使用example_kernel_emmc.uuu 修改为附件的烧录文件uuu_emmc.uuu。

内核与BootLoader在Ubuntu14.04下编译完毕后,cmd命令行使用uuu.exe uuu_emmc.uuu烧录(在Windows 10下操作 uuu.exe SDPS: boot -f u-boot.bin 现象相同)。提示:

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.102-0-gb078bd0
Success 0    Failure 1

1:513    1/ 1 [HID(W):LIBUSB_ERROR_IO                ] SDPS: boot -f u-boot.bin
Error: HID(W):LIBUSB_ERROR_IO
其中u-boot.bin为2018.03编译出的boot文件。
查找问题数日,无果。
请求大牛可以给些建议。
Tags (1)
0 Kudos
Reply
2 Replies

2,655 Views
joanxie
NXP TechSupport
NXP TechSupport

I have replied your another same case, you can follow that one, any update, pls reply there

0 Kudos
Reply

2,472 Views
yibhan
Contributor III

Hi Joanxie,

 

I have a same issue, Do you have a solution to fix that?

My error is : 

[HID(W):LIBUSB_ERROR_IO ] SDPS: boot -f imx-boot-imx8qxpmek-sd.bin-flash

Is there any different way to flash image in imx8qxp?

 

0 Kudos
Reply