imx8qxp uboot logo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp uboot logo

487 Views
myy
Contributor II

Hi,NXP

we use imx8qxp platform,and we want use mipi dsi to display a logo in uboot,Whether patch is available to support it

Our current problem is that the dPU initialization fails  [imxdpuv1.c]

"Error" handler, esr 0xbf000002
elr: 0000000080076f20 lr : 00000000800780a4 (reloc)
elr: 0000000087f14f20 lr : 0000000087f160a4
x0 : 0000000085cab500 x1 : 0000000085cab540
x2 : 0000000000000020 x3 : 0000000000000010
x4 : 0000000000000010 x5 : 0000000000000030
x6 : 0000000087f1e3bb x7 : 00000000ffffffd8
x8 : 000000000000000d x9 : 0000000000000008
x10: 000000000000000d x11: 0000000000000006
x12: 000000000001869f x13: 0000000000010170
x14: 0000000085cab89c x15: 00000000ffffffff
x16: 0000000000000000 x1700
x18: 0000000085cbd590 x19: 0000000000000114
x20: 000000cc
x22: 0000000087f231e0 x23: 0000000087f231cc
x24: 00000000
x26: 0000000000000000 x27: 0000000000000000
x28: 000000000 x29: 0000000085cab4b0

0 Kudos
2 Replies

482 Views
igorpadykov
NXP Employee
NXP Employee

Hi

 

>mipi dsi to display a logo in uboot,Whether patch is available to support it

 

unfortunately such patch is not available, sorry.

 

Best regards
igor

0 Kudos

480 Views
myy
Contributor II

Hi

Check whether the successful logo is displayed in the IMX8QXP uboot?

0 Kudos