imx8qxp recovery mode support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8qxp recovery mode support

533 次查看
TKayO
Contributor III

Hello, 

 

I need the imx8qxp version of below KB article.

How to Support Recovery Mode for POR Reboot Based on i.MX6 Android R13.4.1

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-Support-Recovery-Mode-for-POR-Reb...

 

I need this as u-boot command on imx8qxp.

My product will covered with steel, waterproof case so I need the way to access

boot mode config without opening my product case.

 

Regards,

Brant

0 项奖励
1 回复

524 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Brant

 

I am afraid such document is not available, one can only use as reference

Figure 5-2. High Level Boot Flow, sect.5.2 Terms, sect.5.11 SD/MMC manufacture mode

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

How to Enable Linux BSP L5.4 on a New iMX8/8X Board

 

Best regards
igor