after I success complie the yocto project Rev. L4.14.98_2.3.1, I build imx-boot image using imx-mkimage.
Next, I use the cmd-command line on win10 to execute " uuu -b emmc_all flash.bin fsl-image-qt5-validation-imx-imx8qxpmek.sdcard" . The message is as follows:
uuu -b emmc_all flash.bin fsl-image-qt5-validation-imx-imx8qxpmek.sdcard
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.139-0-g1a8f760
Success 0 Failure 0
1:3 1/ 1 [=================100%=================] SDPS: boot -f flash.bin
but on the board , the bootlaoder stuck on SDP: initialize..., The message is as follows:
U-Boot SPL 2018.03-4.14.98-2.3.3+gc20c44482b (Jun 21 2021 - 01:56:37 +0000)
Normal Boot
Trying to boot from USB SDP
1 setufp mode 0
1 cdns3_uboot_initmode 0
SDP: initialize...
i wait for about half of an hour, the bootloader still hang on SDP: initialize...
Now, I have no idea to solve it, can you give some advice?
Solved! Go to Solution.
hi,
thank you for your support.
the problem is fixed.
The default one or the one you build yourself?
Which bootloader are you using?
hi,
thank you for your support.
the problem is fixed.