imx8qxp m4 hangs at linux boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp m4 hangs at linux boot

1,841 Views
angelo_d
Senior Contributor I

Hi,

once loaded a cortex M4 image at u-boot (bootaux) and checked it works by interacting on the M4 console, i boot linux (boot cmd) and suddenly M4 stops to work. Is this normal ? Is there a way to keep M4 running over Linux boot ?

 

0 Kudos
Reply
6 Replies

1,811 Views
angelo_d
Senior Contributor I

Hi Igor,

sorry, should have been a typo, i tested with   fdt_file=imx8qxp-mek-dsi-rm67191-rpmsg.dtb 

Same issue, M4 app stops to work as soon as the kernel boots, as some clocks or power is cut.

 

 

 

0 Kudos
Reply

1,829 Views
igorpadykov
NXP Employee
NXP Employee

Hi spectrum

 

what bsp used in the case, one can try with latest Linux 5.4.70_2.3.0​, use below dts

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qxp-mek-...

linux documentation

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos
Reply

1,824 Views
angelo_d
Senior Contributor I

Hi Igor,

thanks for the feedback, but issue is still the same: at the moment when linux boots, M4 application stops to run.
I tested a mainline kernel, and it does not stops M4 at boot.

I am using 

imx_5.4.70_2.3.0
imx8qxp-mek-dsi-rm67191.dtb

On M4, i am keeping running  power_mode_switch app, that allows to use an interactive menu on M4 console, and i can see if M4 is running.

From u-boot, i do :

fatload mmc 1:1 ${loadaddr} power_mode_switch.bin && dcache flush && bootaux ${loadaddr} 0

 

(M4 demo works just after fw loading)

command line: console=ttyLP0,115200 root=/dev/mmcblk1p2 rootwait rw

 

As defconfig using one based on imx_v8_defconfig.

If any help, welcome.

Angelo

0 Kudos
Reply

1,815 Views
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

 

could you try imx8qxp-mek-dsi-rm67191-rpmsg.dts as was suggested.

 

Best regards
igor

 

0 Kudos
Reply

1,809 Views
angelo_d
Senior Contributor I

Hi Igor,

 

re-adding here, tested  i tested imx_5.4.70_2.3.0 with   fdt_file=imx8qxp-mek-dsi-rm67191-rpmsg.dtb , still M4 stops to run at kernel boot.

i tested now imx_4.19.35_1.1.0, it does not stop M4 at boot.

So issue is related to imx_5.4.70_2.3.0.  Please let me know if this is an open  issue on imx_5.4.70_2.3.0.

0 Kudos
Reply

1,791 Views
angelo_d
Senior Contributor I

Hi,

seems something related my image built on dunfell and meta-freescale was causing the issue.
Probably something related to SCU fw.

Building using meta-nxp stuff (zeus, using 5.4.70_2.3.0) 

 MACHINE=imx8qxpmek source imx-setup-release.sh -b initial_build_dir 

All seems to work.

 

Thanks

regards

Tags (1)
0 Kudos
Reply