imx8qxp android11 bluetooth can't open

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qxp android11 bluetooth can't open

514件の閲覧回数
c-luo
Contributor III

hi,Dear NXP:

  I have a problem on im8qxp android11 system. I use ap6275 modem.

 I use hci tool I can open bluetooth

such as:

mek_8q:/ # ./data/hciconfig
hci0: Type: BR/EDR Bus: UART
BD Address: D4:9C:DD:DD:23:BF ACL MTU: 1021:8 SCO MTU: 64:1
UP RUNNING
RX bytes:1494 acl:0 sco:0 events:86 errors:0
TX bytes:936 acl:0 sco:0 commands:86 errors:0

mek_8q:/ # ./data/hci
hciconfig hcidump hcitool
mek_8q:/ # ./data/hcitool dev

Devices:
hci0 D4:9C:DD:DD:23:BF

 

but I in android setting, I can‘t open ,and tell me app crash. I look log found uart not dowmload .hcd file.

I want to know libbt-vendor.so  decide whether to download firmware? or I should modify the rest?

I have uploaded the log.

Thanks!

ラベル(1)
0 件の賞賛
返信
0 返答(返信)