imx8mq-evk use the PCM1773 audio codec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mq-evk use the PCM1773 audio codec

316件の閲覧回数
i_MX51
Contributor II

Dear 

When i use the PCM1773 audio codec on my board, it can't work on the android 11, it can work on the android 9 after modify the imx-wm8524, but now android 11 remove the imx-wm8524 from the kernel/sound/soc/fsl/ , so that, when i use the default settings wm8524.c and the simple-card.c, it is fine when i use the tineplay to play wav file, but it haven't sound   when i use the android' player to play the wav or mp4 files.

the below is the tinyalsa_hal error message, please help to check what's the problem.

BR & Thanks

05-12 06:35:30.908 357 2007 D audio_hw_primary:  start_output_stream: pcm_open: card: -1, pcm_device_id: 0, rate: 48000, channel: 2, format: 0, period_size: 0xc0, flag: 8
05-12 06:35:30.908 357 2007 E audio_hw_primary: start_output_stream: Invalid PCM card id: -1

 

ラベル(1)
0 件の賞賛
返信
0 返答(返信)