imx8mq evk sdma firmware not ready?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mq evk sdma firmware not ready?

2,451 Views
gaobo
Contributor I

kernel:4.14.78

rootfs:Ubuntu18.04

machine:imx8mq-evk

Before that, I used the yocto project provided by NXP to compile the image.After burning it to the development board, all peripheral functions can be used.But now I use Ubuntu 18.04 file system to replace the file system in NXP demo, resulting in Bluetooth and sound card problems。( imx-sdma 30bd0000.sdma: sdma firmware not ready!)

pastedImage_5.png

pastedImage_6.png

I don't think it's a driver problem, but I'm not sure what's wrong.

please give me some advise,thanks!

0 Kudos
Reply
2 Replies

1,801 Views
lebeer
Contributor II

Hi:

您好,您遇到的这个问题解决了吗?我也遇到

您方便时看下这个是什么原因。

Re: i.MX8MQ UART 串口不能通讯的问题 - NXP Community

0 Kudos
Reply

2,192 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, Ubuntu Rootfs is not supported by us. I apologize for the inconvenience this may give you.

Best regards,

Diego.

0 Kudos
Reply