imx8mq evk + samsung HDR TV

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mq evk + samsung HDR TV

610件の閲覧回数
nagendrasarma
Contributor III

hi NXP

we are using SAMSUNG 4k tv (version BA01 supports HDR )  with IMX8mq-evk 

the hdmi is not working and xwayland window is not coming on the tv 

showing hdmi plug in and hdmi plug out error on console 

the tv is detecting the device connected to it .like PC and settop box etc 

but the IMx8evk is not being detected by the tv and saying unknown device ?

could you please support us to resole this ? what could be wrong ?

we are using yocto xwayland image 

note: old samsung 4k tv is working with imx8mq-evk 

regards

Nagendra

タグ(1)
0 件の賞賛
2 返答(返信)

422件の閲覧回数
nagendrasarma
Contributor III

Hi Bio,

thanks for suggestion, I tried with all ports available with TV and unfortunately none of them working 

the new samsung tv is detecting the hdmi device connected to it. (like PC and settp box etc)

do we need to enable  anything to support this detection in IMX hdmi-fw or hdmi driver ?

fyi:  also tried with disabling  CEC  ,hdcp options on imx side

regards,

Nagendra 

0 件の賞賛

422件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi nagendra,

I just can say to try to connect on another port, there is no report that MX8M works on one 4K Monitor and other no.

0 件の賞賛