I am trying to build imx-yocto-L4.14.98_2.0.0_ga following the instructions in "i.MX_Linux_User's_Guide.pdf".
My host machine runs Ubuntu 16.04.
The build configuration is as follows:
DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source fsl-setup-release.sh -b output_imx8mmevk
bitbake fails reporting there is no kernel provider for the machine.
I have copied the output from bitbake below.
I get the same result with both imx-4.14.98-2.0.0_ga.xml and imx-4.14.98-2.0.1_patch.xml.
I went through these exact steps two months ago approx without any problem.
bitbake fsl-image-validation-imx
Parsing recipes: 100% |##########################################| Time: 0:01:00
Parsing of 2563 .bb files complete (0 cached, 2563 parsed). 3484 targets, 224 skipped, 8 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing PROVIDES 'virtual/kernel'
linux-toradex PROVIDES virtual/kernel but was skipped: incompatible with machine imx8mmevk (not in COMPATIBLE_MACHINE)
...
linux-imx PROVIDES virtual/kernel but was skipped: incompatible with machine imx8mmevk (not in COMPATIBLE_MACHINE)
...
linux-fslc-imx PROVIDES virtual/kernel but was skipped: incompatible with machine imx8mmevk (not in COMPATIBLE_MACHINE)
...
linux-yocto-tiny PROVIDES virtual/kernel but was skipped: incompatible with machine imx8mmevk (not in COMPATIBLE_MACHINE)
ERROR: Required build target 'fsl-image-validation-imx' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-validation-imx', 'virtual/kernel']
解決済! 解決策の投稿を見る。
Apologies, mea culpa. This error was entirely my fault, the case can be closed.
Can you explain what was your error, what exactly did you do wrong?
I am facing a similar error when I try to build the image with yocto of the board MBLS1028A-IND.