Hi.
There are two different registers which have settings for the P, M and S dividers associated with the MIPI DSI interface PLL:
GPR_MIPI_M_PLLPMS (part of DISPLAY_BLK_CTRL at base address 32E2_8000h) has PMS_P, PMS_M, PMS_S.
DSI_PLLCTRL (part of MIPI_DSI at base address 31E1_0000h) has PMS.
First question: how do these two registers relate to one another?
I would like to use spread spectrum with the display interface. The Linux driver drivers/gpu/drm/bridge/sec-dsim.c uses the second of the two registers indicated above to set PMS. However, the SSCG_EN bit to enable spread spectrum is part of GPR_MIPI_M_PLLCTL_LOW.
Second question: If setting the SSCG_EN bit, do the PLL divisors have to be set up using the DISPLAY_BLK_CTRL block, or can SSCG_EN be set in GPR_MIPI_M_PLLCTL_LOW while the above driver sets up the rest of the PLL?
Or more generally, how does one initialize the PLL when using spread spectrum?
Thanks,
Steve
解決済! 解決策の投稿を見る。
For P, M, S, we stuck with DSI_PLLCTRL as is written by the Linux driver drivers/gpu/drm/bridge/sec-dsim.c.
For the spread spectrum part we found that using the GPR_MIPI_M_PLLCTL_LOW and _HIGH registers does not work. No dither was observed. However, one of the other guys figured out that using DSI_PLLCTRL1 and DSI_PLLCTRL2 (32E1_0098, 32E1_009C) does work. The RM does not detail the bits in those registers, but using the arrangement described for GPR_MIPI_M_PLLCTL_LOW and GPR_MIPI_M_PLLCTL_HIGH worked.
For P, M, S, we stuck with DSI_PLLCTRL as is written by the Linux driver drivers/gpu/drm/bridge/sec-dsim.c.
For the spread spectrum part we found that using the GPR_MIPI_M_PLLCTL_LOW and _HIGH registers does not work. No dither was observed. However, one of the other guys figured out that using DSI_PLLCTRL1 and DSI_PLLCTRL2 (32E1_0098, 32E1_009C) does work. The RM does not detail the bits in those registers, but using the arrangement described for GPR_MIPI_M_PLLCTL_LOW and GPR_MIPI_M_PLLCTL_HIGH worked.
if you need set P, M,S, set the GPR register, I mean GPR_MIPI_M_PLLPMS