Hi,
We have designed imx8m mini custom board.
imx8m mini evk contains Sandisk(SDINBDG4-16G-I1) 16gb emmc connected to SD3 interface.
Our custom contains Micron(MTFC8GAMALBH-AIT) 8gb emmc connected to SD3 interface.
What are code needs to change from spl, uboot, kernal in order to boot from micron 8gb emmc ?
Thanks & Regards,
Vasu
No changes in the code seem to be required. You just have to load spl, uboot and kernel binaries from the beginning of the flash memory address space in the regular way and then appropriately create a partition for the rootfs in the rest of the flash memory space.
Best Regards,
Artur