imx8m GPRs for MIPI DSI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8m GPRs for MIPI DSI

1,216 次查看
guido_gunther
Contributor II

The IOMUXC GPR23-GPR34 registers contain DSI related bits but they only state e.g. "for DSI control", "for DSI test status" or "for DSI status" not telling me what they're supposed to do. Are there any details?

The kernel sources seem to only refer to IMX8MQ_GPR13_MIPI_MUX_SEL for muxing between DCSS and LCDIF.

Any details would be greatly appreciated!

标记 (2)
0 项奖励
3 回复数

732 次查看
art
NXP Employee
NXP Employee

The bits you are talking about are for factory testing purposes only and should not be used during regular operation.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

732 次查看
guido_gunther
Contributor II

The bits you are talking about are for factory testing purposes only and should not be used during regular operation.

The sound useful for LCD panel bringup / debugging though. Any chance you can provide any details?

0 项奖励

732 次查看
guido_gunther
Contributor II

Seems there's more interest in documentation for these registers: https://community.nxp.com/thread/471203 

0 项奖励