imx8dx libsdl2 color display problem

cancel
Showing results for 
Search instead for 
Did you mean: 

imx8dx libsdl2 color display problem

207 Views
songhongliang
Contributor II

HI

I am trying to use libsdl2, but the windows created with SDL2 on the imx8dx development board are showing wrong colors. Compared with using the same program on ubuntu, the display on Ubuntu is normal, and the color displayed on the imx8dx development board is always wrong. I added in conf/local.conf IMAGE_INSTALL_append += "libsdl2 libsdl2-net libsdl2-mixer libsdl2-ttf libsdl2-image"

 

Thanks!

0 Kudos
2 Replies

176 Views
Sanket_Parekh
NXP Employee
NXP Employee

Hi @songhongliang 

I hope you are doing well.

Please try with libsdl.

Thanks & Regards

Sanket Parekh

0 Kudos

205 Views
songhongliang
Contributor II

hi

Attached is the comparison shown above on Ubuntu and imx8dx

Thanks

Tags (1)
0 Kudos