imx8 nano - usdhc3( emmc ) reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8 nano - usdhc3( emmc ) reset

690件の閲覧回数
razriel
Contributor II

Our custom board is based on imx8mn-ddr4-evk with slight modifications.

Currently board is loading u-boot, kernel and rootfs when boot mode is set to SD-CARD and usdhc3 ( is disabled)

When udshc3( emmc ) is enabled in device tree the u-boot fails. system restart without any warnning in debug terminal.

We have verified pins allocation and routing of eMMC is same as refrence design. We are having hard time to figure out what causes the target board to restart during the run of the u-boot.

This issue prevents us from being able to flash the emmc from uuu in boot download mode. Our goal is to  be able to load the system from eMMC boot mode.

Next step we plan is to connect Jlink/JTAG to run u-boot step by step and learn where the firmware crashes. 

please help if you have any idea what can cause such a behaviour. 

 

 

0 件の賞賛
3 返答(返信)

674件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

For your design you need to enable the usdhc3 in the software then it can work. Here you can refer to https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enabling-uSDHC1-of-i-MX8MM-Based-On-L5-4... this threads. It will help you.

0 件の賞賛

664件の閲覧回数
razriel
Contributor II
ushdc3 is enabled and working on EVK. same pinout same flash part number on target board. but on target board it crashes in the middle of u-boot run. the is no message in debug terminal before it restarts.
0 件の賞賛

663件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you finished all the configuration for the EMMC? And when you download image to emmc, is there information on the debug terminal?

0 件の賞賛