imx8 M4 access to SAI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8 M4 access to SAI

709 次查看
isa_leo
Contributor I
Hi, We are working on audio application project using the iMX8QM and are planning to use the M4s running FreeRTOS for the real-time audio processing aspect of the application and use the other A53/A72 cores running Linux for upper level stuff. From the iMX8 block diagram, the Audio subsystem seems to be accessible by the M4s. We search for documentations to get more details about this but couldn't find much. So my questions are: - Is it possible for the SAI or ESAI to be used by the M4s ? - If so, is there a SAI and/or ESAI driver for the M4 available from NXP or somewhere else that can get us started ? Thanks, LM
0 项奖励
2 回复数

691 次查看
nxf54947
NXP Employee
NXP Employee

Hello @isa_leo,

You may refer to the MCUXpresso SDK for i.MX8QM-MEK, which is a available through the MCUXpresso SDK Builder. This an SDK which enables the Cortex-M4 core functionality on the i.MX 8QM.

Once you downloaded the SDK, please find two driver examples for ESAI and SAI on this path:

\boards\mekmimx8qm\driver_examples

Hope this helps!

Regards,

Ruben

0 项奖励

688 次查看
isa_leo
Contributor I

Hi Ruben,

Ok. Thanks for the suggestion. We'll look it up.

 

Cheers,

LM

0 项奖励