imx7ulpevk i2c bus devices?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx7ulpevk i2c bus devices?

709件の閲覧回数
Raxesh-Oriya
Contributor III

I am unable to find out devices shown by i2cdetect utility for i2c-0. I looked at schematics (spf-29163_b2 & SPF-29164_B1) as well.

Device address on bus(i2c-0): 0x1d, 0x38, 0x3f

Base Board: MCIMX7ULP-EVK REV B1

RaxeshOriya_0-1628062231721.pngRaxeshOriya_1-1628062255968.png

Any lead?

ラベル(3)
0 件の賞賛
2 返答(返信)

687件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

I cannot find any reference for 2 of the 3 address that you are seeing, I believe that 0x38 correspond to the Focaltech touch panel.

I would like to know which BSP version are you using for your test?
Do you have anything connected to the Arduino and/or MFI connector?

Best regards,
Aldo.

0 件の賞賛

676件の閲覧回数
Raxesh-Oriya
Contributor III

Hi @AldoG,

Thanks for your reply. Correct, 0x38 correspond to the Focaltech touch panel but that is on i2c-1 and NOT on i2c-0(which I attached image in my first post). Here is the result of i2c-1:

RaxeshOriya_0-1629172535785.png

I am using my own Yocto distro which includes meta-freescale layer and I do not have anything connected to the Arduino and/or MFI connector.

0 件の賞賛