Hi:
My customer want to support the bcm4339 ap mode in imx7d sabresd board, i have download the demo images:L4.9.11_1.0.0-ga_images_MX6UL7D.tar.gz.
But i doesn't support the ap mode, because this demo images doesn't provide the AP mode firmwares.
I can see only these files in /lib/firmware/bcm/ZP_BCM4339/:
bcmdhd.ZP.OOB.cal bcmdhd.ZP.SDIO.cal fw_bcmdhd.bin fw_bcmdhd_mfgtest.bin.
In my understand, bcm4339 should load the firmware "fw_bcmdhd_apsta.bin" to enable ap mode.
Could you provide the fw_bcmdhd_apsta.bin of linux 4.9.11_1.0.0-ga.
By the way, the firmware load PATH has tow items:
CONFIG_BCMDHD_FW_PATH="/lib/firmware/bcm/ZP_BCM4339/fw_bcmdhd.bin"
CONFIG_BCMDHD_NVRAM_PATH="/lib/firmware/bcm/ZP_BCM4339/bcmdhd.ZP.OOB.cal"
For supporting wifi ap mode, /lib/firmware/bcm/ZP_BCM4339/bcmdhd.ZP.OOB.cal is also need to replace with AP mode files?
Regards,
czou
Hi czou
please check thread where that file was generated
iMX6 YOCTO 4.1.15-1.2.0 doesn't generate bcmdhd.ko (Murata drivers)
also one can try to ask help on Murata support
wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------