imx7 defconfig and imx_v7_defconfig

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7 defconfig and imx_v7_defconfig

3,091 Views
carlosbejar-col
Contributor I

Dear NXP Community,

I have imx7dsabresd board and was able to build yocto from fsl-community-bsp and loaded fine (kernel: linux-imx_4.1.15)

Now, I want to modify the kernel config and before doing that just want to understand how the two defconfig files are used by yocto to generate the ".config" file.

meta-freescale/recipes-kernel/linux/linux-imx-4.1.15/imx/defconfig
kernel source tree: arch/arm/configs/imx_v7_defconfig

Could you point me the recipe(s) or documentation that I can go throught?

Thanks,
Carlos

0 Kudos
1 Reply

1,791 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the following regarding Building Linux Kernel 

Also, please look at the following :

Kernel config file used by Yocto 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos