Hi,
I've created a custom imx6ull board and therefore copied dts from imx6ul-14x14 evk board.
In this dts file, there are 3 pinctrl for "default", 100MHz and 200MHz.
Current result of cat /sys/kernel/debug/mmc0/ios is:
clock: 50000000 Hz
actual clock: 49500000 Hz
vdd: 21 (3.3 ~ 3.4 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 2 (4 bits)
timing spec: 2 (sd high-speed)
signal voltage: 0 (3.30 V)
driver type: 0 (driver type B)
How is it possible to increase clock and speed? Which settings have to be changed?
Currently, read from sd card is quite slow.
Thx!
Alexander
Hi Alexander
linux driver selects maximum speed automatically based
on sd csd register maximum data transfer rate, so for example sd1 port
has 3 pinctrl for "default", 100MHz and 200MHz. Note for such high rates
power cycling is needed, provided by SD1_nRST.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Ok, clear.
And what about BOOT_CFG1? Does it makes sense to change [2,3] to increase speed? If yes, is it possible to test these settings without ordering a new pcb? Like in fuse or any other settings?
Thank you for your answer.
How do I set the eFUSE? Without destroying all other parts :smileywink:
All boot parameters are defined by resistors on boot (LCD_... Pins) but SDR50 or SDR104 has to be set by eFUSE.
Thx,
Alexander