My DTS configuration is as follows:
clocks {
codec_osc: codec_osc {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <12000000>;
};
};
vgen4_reg: vgen4 {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
reg_3p3v: 3p3v {
compatible = "regulator-fixed";
regulator-name = "3P3V";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
sound-sgtl5000 {
compatible = "fsl,imx6ul-arm2-sgtl5000",
"fsl,imx-audio-sgtl5000";
model = "imx6ul-arm2-sgtl5000";
cpu-dai = <&sai2>;
audio-codec = <&codec>;
audio-routing =
"LINE_IN", "Line In Jack",
"Headphone Jack", "HP_OUT";
};
&i2c1 {
codec: sgtl5000@0a {
compatible = "fsl,sgtl5000";
reg = <0x0a>;
clocks = <&codec_osc>;
VDDA-supply = <&vgen4_reg>;
VDDIO-supply = <®_3p3v>;
};
}
&sai2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai2>;
assigned-clocks = <&clks IMX6UL_CLK_SAI2_SEL>,
<&clks IMX6UL_CLK_SAI2>;
assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <0>, <12288000>;
status = "okay";
};
Why every time you start to make an error, leading to sgtl5000 registration failed, The error function occurs in the read I2C function,Functions are as follows:
/* read chip information */ |
ret = regmap_read(sgtl5000->regmap, SGTL5000_CHIP_ID, ®);
if (ret)
goto disable_clk; |
I2C on the other devices work properly, what is the cause of the failure of the sgtl5000 registration? Thank you!
Hi igor,
I am facing the same issue in our imx6ul target board with sgtl5000 audio codec. MCLK is not coming from SOC. Please suggest me some solution.
Hi Ferdi,
please share the changes if you've already fixed this issue.
Below for log information
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
sgtl5000_i2c_probe addr:a, name:sgtl5000
sgtl5000: probe of 0-000a failed with error -5
fsl-asrc 2034000.asrc: driver registered
imx6ul-pinctrl 20e0000.iomuxc: pin MX6UL_PAD_GPIO1_IO08 already requested by 20e0000.iomuxc; cannot claim for 2004000.spdif
imx6ul-pinctrl 20e0000.iomuxc: pin-31 (2004000.spdif) status -22
imx6ul-pinctrl 20e0000.iomuxc: could not request pin 31 (MX6UL_PAD_GPIO1_IO08) from group spdifgrp on device 20e0000.iomuxc
fsl-spdif-dai 2004000.spdif: Error applying setting, reverse things back
imx-sgtl5000 sound-sgtl5000.15: ASoC: CODEC (null) not registered
imx-sgtl5000 sound-sgtl5000.15: snd_soc_register_card failed (-517)
platform sound-sgtl5000.15: Driver imx-sgtl5000 requests probe deferral
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)
gpio_dvfs: disabling
vref-3v3: disabling
can-3v3: disabling
SD2_SPWR: disabling
SD1_SPWR: disabling
regulator-dummy: disabling
imx mcc test is registered.
imx-sgtl5000 sound-sgtl5000.15: ASoC: CODEC (null) not registered
imx-sgtl5000 sound-sgtl5000.15: snd_soc_register_card failed (-517)
platform sound-sgtl5000.15: Driver imx-sgtl5000 requests probe deferral
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
imx-sgtl5000 sound-sgtl5000.15: ASoC: CODEC (null) not registered
imx-sgtl5000 sound-sgtl5000.15: snd_soc_register_card failed (-517)
ALSA device list:
platform sound-sgtl5000.15: Driver imx-sgtl5000 requests probe deferral
No soundcards found.
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk1p2): using internal journal
EXT3-fs (mmcblk1p2): recovery complete
EXT3-fs (mmcblk1p2): mounted filesystem with ordered data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 388K (809a3000 - 80a04000)
INIT: version 2.88 booting
scsi 0:0:0:0: Direct-Access Generic Flash Disk 8.07 PQ: 0 ANSI: 4
sd 0:0:0:0: [sda] 1966080 512-byte logical blocks: (1.00 GB/960 MiB)
imx-sgtl5000 sound-sgtl5000.15: ASoC: CODEC (null) not registered
imx-sgtl5000 sound-sgtl5000.15: snd_soc_register_card failed (-517)
Hi ferdi
for sgtl5000 i2c failure on can check its erratum
http://cache.freescale.com/files/analog/doc/errata/SGTL5000ER.pdf
and if SION bit is set in pinctrl, then test with oscilloscope i2c signals,
add some printfs to probe function. For dts example one can use
i.MX6SX, as it has the same sai module
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------