imx6ul tf card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ul tf card

678 次查看
songyonglai
Contributor II
Hi Igorpadykov: On my board, I use the usdhc2 to connect a emmc to boot from, and use the usdhc1 to connect a SD(TF) card, when I plug a TF card, the kernel can detect it ,but can not attach successfully. I debug the kernel and find a error in sdhci_cmd_irq() ,the error is SDHCI_INT_DATA_END_BIT(this is defined in file sdhci.h of kernel file). So I don't know why this error occurs. (I use the imx6ul-14*14-evk.dts). Igorpadykov ,would you help me and give me some suggestions, thanks very much .
0 项奖励
回复
3 回复数

662 次查看
songyonglai
Contributor II

Hi  Igorpadykov:

  Thanks for your reply. It seems that my problem is not same with the one you discussed above. I think if SD1 cmd and clock pinmux value were not set correct. In dts file imx6ul-14*14-evk.dts, I usethe pinmuxs as follows referenced from demo board:

  pinctrl_usdhc1:usdhc1grp{

     MX6UL_PAD_SD1_CMD_USDHC1_CMD 0x17059

     MX6UL_PAD_SD1_CLK_USDHC1_CLK 0x10071

     MX6UL_PAD_SD1_DATA0_USDHC1_DATA0 0x17059

     MX6UL_PAD_SD1_DATA1_USDHC1_DATA1 0x17059

     MX6UL_PAD_SD1_DATA2_USDHC1_DATA2 0x17059

     MX6UL_PAD_SD1_DATA3_USDHC1_DATA3 0x17059

 

So, are the values above acorrding to the hardware designing? and shouled I modify them?

 

Thanks very much.

0 项奖励
回复

658 次查看
igorpadykov
NXP Employee
NXP Employee

>values above acorrding to the hardware designing? and shouled I modify them?

 

this depends on custom board layout, so you should find correct settings (drive strength) yourself

based on suggestions provided on reference link with similar issue.

 

Best regards
igor

 

0 项奖励
回复

672 次查看
igorpadykov
NXP Employee
NXP Employee

Hi songyonglai

 

such error was reported on other forums like https://forums.developer.nvidia.com/t/debugging-sd-uhs-cards-on-the-tx2/67641/3

and seems it is related to signal integrity, so one can try solutions for improving signal quality suggested on

https://community.nxp.com/t5/i-MX-Processors/eMMC-8GB-to-4GB-crash-on-linux-yocto-boot/m-p/373231

 

Best regards
igor

0 项奖励
回复