hi,
I'm testing the camera of i.mx6ul,Test steps are as follows:
insmod /lib/modules/3.14.38-6UL_ga+ge4d0573/kernel/drivers/media/platform/mxc/subdev/mx6s_capture.ko
insmod /lib/modules/3.14.38-6UL_ga+ge4d0573/kernel/drivers/media/platform/mxc/subdev/ov5640_camera.ko
A serial port output:
1-003c supply DOVDD not found, using dummy regulator
1-003c supply DVDD not found, using dummy regulator
1-003c supply AVDD not found, using dummy regulator
CSI: Registered sensor subdevice: ov5640 1-003c
camera ov5640, is found
then,use this command:/unit_tests/mx6s_v4l2_capture.out -d /dev/video1 -m 1
the lcd output is deranged,
Please advise.
Thank you
解決済! 解決策の投稿を見る。
Hi,
1)
Have you checked the caps of imxv4l2src?
gst-inspect-1.0 imxv4l2src
You have to use available configurations:
Capabilities:
video/x-raw
format: YUY2
width: 640
height: 480
framerate: { 15/1, 30/1 }
video/x-raw
format: YUY2
width: 320
height: 240
framerate: { 15/1, 30/1 }
video/x-raw
format: YUY2
width: 720
height: { 576, 480 }
framerate: { 15/1, 30/1 }
video/x-raw
format: YUY2
width: 1280
height: 720
framerate: { 15/1, 30/1 }
video/x-raw
format: YUY2
width: 1920
height: 1080
framerate: 15/1
video/x-raw
format: YUY2
width: 2592
height: 1944
framerate: 15/1
video/x-raw
format: YUY2
width: 176
height: 144
framerate: { 15/1, 30/1 }
video/x-raw
format: YUY2
width: 1024
height: 768
framerate: { 15/1, 30/1 }
2) For example:
gst-launch-1.0 -v imxv4l2src device=/dev/video1 ! "video/x-raw, format=(string)YUY2, width=(int)640, height=(int)480, framerate=(fraction)15/1" ! videoconvert ! x264enc ! avimux ! filesink location=webcam.avi
Check the Linux user Guide, multimedia section.
Luis
thanks!
i try this command
root@imx6ulevk:~# gst-launch-1.0 imxv4l2src device=/dev/video1 ! imxv4l2sink
====== IMXV4L2SRC: 4.0.7 build on Jan 18 2016 16:19:53. ======
set color key:00010203
====== IMXV4L2SINK: 4.0.7 build on Jan 18 2016 16:19:53. ======
Setting pipeline to PAUSED ...
display(/dev/fb0) resolution is (800x600).
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
v4l2sink need allocate 3 buffers.
but,Phenomenon is the same, in a moving picture can faintly see a little bit image
Hello,
It looks a hardware problem as the module I tested works fine.
https://community.freescale.com/thread/379349
Luis
hi,
I added a capacitance in CSI_VSYNC feet Can display now, but there's the red noise, I want to look at the effect of the photo?Have a test photos and video of the order?
Hello,
What do you need exactly?
Luis
hi,
I want the Take photos or video test order, I want to see if there are any more noise out photos。I want to take a photo。
luis,
thank you!
I also took a picture, I found is not very clear Whether to focus, I also want to know how to take pictures of the different resolutions
What is the orders of the video?
There is a problem I'm using the command“ gplay-1.0 test. mp4” LCD without picture, only the sound。
Hi,
You can introduce caps in the pipeline for different resolutions. "video/x-raw, format=(string)YUY2, width=(int)640, height=(int)480, framerate=(fraction)15/1"
Like :
gst-launch-1.0 -v imxv4l2src device=/dev/video1 ! "video/x-raw, format=(string)YUY2, width=(int)640, height=(int)480, framerate=(fraction)15/1" ! imxv4l2sink
How did you create the test.mp4?
Luis
Hi,luis,
1,2592 x1944 resolution is not successful,the other is ok.
gst-launch-1.0 -v imxv4l2src device=/dev/video1 ! "video/x-raw, format=(string)YUY2, width=(int)2592, height=(int)1944, framerate=(fraction)15/1" ! imxv4l2sink
and taking pictures is the same:
gst-launch-1.0 imxv4l2src num-buffers=1 device=/dev/video1 ! "video/x-raw, format=(string)YUY2, width=(int)2592, height=(int)1944, framerate=15/1" ! jpegenc ! filesink location=test.jpg
2,Test. Mp4 is downloading video file,Is there any requirement for broadcast file? Can you give a reference test command?
Hello,
1. Is that resolution supported by your sensor?
2. I am sorry, I don't understand what you need. Do you want to play a mp4 file? Create your own file with camera?
Luis
Hi,
1)
Have you checked the caps of imxv4l2src?
gst-inspect-1.0 imxv4l2src
You have to use available configurations:
Capabilities:
video/x-raw
format: YUY2
width: 640
height: 480
framerate: { 15/1, 30/1 }
video/x-raw
format: YUY2
width: 320
height: 240
framerate: { 15/1, 30/1 }
video/x-raw
format: YUY2
width: 720
height: { 576, 480 }
framerate: { 15/1, 30/1 }
video/x-raw
format: YUY2
width: 1280
height: 720
framerate: { 15/1, 30/1 }
video/x-raw
format: YUY2
width: 1920
height: 1080
framerate: 15/1
video/x-raw
format: YUY2
width: 2592
height: 1944
framerate: 15/1
video/x-raw
format: YUY2
width: 176
height: 144
framerate: { 15/1, 30/1 }
video/x-raw
format: YUY2
width: 1024
height: 768
framerate: { 15/1, 30/1 }
2) For example:
gst-launch-1.0 -v imxv4l2src device=/dev/video1 ! "video/x-raw, format=(string)YUY2, width=(int)640, height=(int)480, framerate=(fraction)15/1" ! videoconvert ! x264enc ! avimux ! filesink location=webcam.avi
Check the Linux user Guide, multimedia section.
Luis
Hi Luis
How did you add the "x264enc" in Yocto? I bitbake fsl-image-qt5 for imx6ul, and i found it haven't x264enc element. could you help me ?
Thanks
yes,i use this device tree
the ov5640 PWDN pin is pull down with 10k resistance,is This have any effect?
Hello,
You can try:
insmod /lib/modules/3.14.38-6UL_ga+ge4944a5/kernel/drivers/media/platform/mxc/subdev/ov5640_camera.ko
insmod /lib/modules/3.14.38-6UL_ga+ge4944a5/kernel/drivers/media/platform/mxc/subdev/mx6s_capture.ko
gst-launch-1.0 imxv4l2src device=/dev/video1 ! imxv4l2sink
Luis
hi, luis,
I found a strange problem, I use the oscilloscope probe to quantity CSI_VSYNC feet, image is clear,But the image will move up
Hi 小辉哥 в
also it may be useful to look at i.MX6SL camera driver, as it also uses CSI-PXP path:
About preview function in i.MX6SL.
Best regards
igor
hi,igir,
thanks
Before I read this article discussion, still want to thank you for your answers.
i
Hello,
Are you ising this device tree?
imx6ul-14x14-evk-csi.dtb
Luis