Hi,
we are making some power consumption tests on the imx6ul evaluation board, and we found something which seems a bit odd. When the board enter the "suspend-on-ram" mode, the total consumption of the board goes from 150 mA to 50 mA.
50mA seems quite a lot for this mode. Do we have to modify anything to optimize the power consumption when in deep-sleep mode?
I read the application note AN5170 (http://cache.freescale.com/files/32bit/doc/app_note/AN5170.pdf?pspll=1 ), and the results are very different.
Our image has been made with yocto.
Regards
解決済! 解決策の投稿を見る。
available low power modes are provided in
Table 14. Low Power Mode Current and Power Consumption
i.MX6UL Datasheet (rev.0, 8/2015)
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf
Best regards
igor
Hi giuliano
AN5170 did not measure whole board consumption and it
has many other components which add current. Measured
VDD_SOC_IN, VDD_HIGH_IN, DDR3L and other processor power
domains with all processor modules are disabled.
Peripheral chips power consumption is not included in measurements.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Oh, my bad!
Is the hibernation mode available for the imx6ul (suspend-on-disk)? And if not, is it in NXP roadmap for this chip?
available low power modes are provided in
Table 14. Low Power Mode Current and Power Consumption
i.MX6UL Datasheet (rev.0, 8/2015)
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf
Best regards
igor