imx6ul evk play music

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ul evk play music

2,221件の閲覧回数
caibai
Contributor III

i use imx6ul evk and yocto,

when i play music like

# gst-play xxx.mp3

and it sounds have noise.

how to solve it??

ラベル(3)
0 件の賞賛
2 返答(返信)

1,716件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI cai

please try commands as in attached Linux Guide sect.7.3.1.1 Audio-only playback

and use  Demo Images on:

Board Support Packages (1)

L3.14.38_iMX6UL (REV L3.14.38_6ul) New

i.MX 6UltraLite Linux Binary Demo Files and Linux BSP Documentation

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,716件の閲覧回数
caibai
Contributor III

thanks for reply.

i run

# gst-launch-1.0 filesrc location=test.mp3  ! id3demux ! queue ! mpegaudioparse ! beepdec ! pulsesink

but it sound the same as i run gst-play xxx.mp3

0 件の賞賛