imx6ul - Tamper functions not working (active tamper, temperature tamper)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul - Tamper functions not working (active tamper, temperature tamper)

1,033 Views
andreasb
Contributor I

Hi!

We are using a imx6ul and want to enable tamper functions s.t. ZMK and LPGPR will be deleted in case of a tamper event. Unfortunately active tamper functions as well as temperature tamper functions are not working at all.

Preconditions:

*) Device is in "Trusted"-State (HAB enabled and device closed)
*) LPPGDR was set and PGD cleared in LPSR as described in Section "Power glitch detector"
*) SRTC is enabled (LPSRTCLR is counting)

*) LPGPR0 is set to a known value


For active tamper functions:
*) ATx_PAD_EN and ATx_EN is enabled in LPATCTLR (for all x = 1 to 5)
*) but we could not measure any output of the LFSR at the Tamper-Pins using a oscilloscope

For temperature tamper functions:

*) DRYICE_EN is set in DTOCR

*) TEMP_DET_EN is set in DMCR
*) TT_EN is set in LPTDCR
*) when the device is cooled below -30°C the tampering is still not detected. (LPGPR0 is not cleared, State not changed, no Flag in LPSR)

Are we missing anything? - Any help would be appreciated!

Labels (1)
0 Kudos
Reply
1 Reply

795 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed

NDA. We cannot discuss this with you in public anyway, this requires to be handled as a Service Request (SR).

Be aware that to give you remote support through a SR, we will still need the confirmation of a NXP employee,

that the NDA is in place.

Support|NXP 


Hello,
Have a great day,
Yuri

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply