imx6uL Watchdog (WDOGX_B)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6uL Watchdog (WDOGX_B)

686 Views
prabhatkumar
Contributor II

In imx6UL, is watchdog (WDOGx_B / WDOG_ANY) enabled by default or need to be enable in software?

If I muxed LCD_RESET [ALT4] pin for watchdog

While power up, uboot failed to load. Will watchdog kick in?

Labels (2)
0 Kudos
1 Reply

557 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prabhat

>In imx6UL, is watchdog (WDOGx_B / WDOG_ANY) enabled by default or need to be enable in software?

yes it should be enabled in software. Also in Serial Downloader mode it can be enabled by

fuse WDOG Timeout Select, this is described in Chapter 8 System Boot Reference Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos