The Linux driver for mcc and M4 linker files use 0xBFF00000 memory address. DDR RAM starts at 0x80000000 and goes to 512M or 1G. 1G(0x3f800000) + 0x8000_0000 is 0xBF800000, According to manual section 2.2 IMX 6SX 8000_0000 to FFFF_FFFF is the MMDC xDDR controller.
- what is the type of memory is being referenced, i.e SRAM, DDR. (the linker files states its DDR) some other mapping?
- is there a Linux driver that creates this mapping?
已解决! 转到解答。
OK.. But it does not go into detail about how the address is setup fro the shared RAM... I've two RAM layouts shown below:
BFF00000 is defined as MCC_BASE_ADDRESS in mcc_config_linux.h
1GB
physical memory 80000000 +
1GB of RAM 40000000 =
top address is C0000000 - BFF00000 = 100000 1MB of RAM
512MB
9ff00000 is defined as MCC_BASE_ADDRESS in mcc_config_linux.h
80000000 + 20000000 = A0000000 - 9ff00000 = 100000
But this does not work.. mcc_get_bookeeping_data crashes using ioremap_nocache
Or I'm not understanding the memory mapping of DDR memory to MCC_BASE_ADDRESS?
Hi Tim
for mapping one can look linux../../arm/mach-imx/hardware.h
mcc driver is described in attached Linux Manual
Chapter 53 i.MX 6 SoloX Multi-Core Communication (MCC)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
OK.. But it does not go into detail about how the address is setup fro the shared RAM... I've two RAM layouts shown below:
BFF00000 is defined as MCC_BASE_ADDRESS in mcc_config_linux.h
1GB
physical memory 80000000 +
1GB of RAM 40000000 =
top address is C0000000 - BFF00000 = 100000 1MB of RAM
512MB
9ff00000 is defined as MCC_BASE_ADDRESS in mcc_config_linux.h
80000000 + 20000000 = A0000000 - 9ff00000 = 100000
But this does not work.. mcc_get_bookeeping_data crashes using ioremap_nocache
Or I'm not understanding the memory mapping of DDR memory to MCC_BASE_ADDRESS?