imx6solo and LPDDR2 Stress Testing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6solo and LPDDR2 Stress Testing

1,862 Views
deepaktajanpure
Contributor II

Hi, I want to do LPDDR2 Stress testing on imx6solo custom board. So will you please provide .inc file or any other utility for doing this. DDR Used is MT42L16M32D1HE-18

23 Replies

913 Views
pengyong_zhang
NXP Employee
NXP Employee

hi @deepaktajanpure 

FIrstly, You do not need to modify the RPA .inc file. Just set the right DDR parameter is OK.

And the RPA file  thay i have sened to you is no issue follow your DDR type. So please check your DDR layout is no problem.

B.R

0 Kudos
Reply

929 Views
pengyong_zhang
NXP Employee
NXP Employee

hi, @deepaktajanpure 

what do you mean enable chip select? what is your each step?

0 Kudos
Reply

928 Views
deepaktajanpure
Contributor II

I just enabled CS0 using below line

setmem /32 0x021b0000 = 0x82010000 // MMDC0_MDCTL

 

which was not there in your previous script

0 Kudos
Reply

948 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @deepaktajanpure 

What so you mean not enabled any chip select? you can see the RPA file.

0 Kudos
Reply

947 Views
deepaktajanpure
Contributor II

After enabling Chip Select I'm getting same error as I posted below. Calibration fails again

0 Kudos
Reply

971 Views
pengyong_zhang
NXP Employee
NXP Employee

hi, @deepaktajanpure 

PLease use the attachment file, And also check your PCB design if is folllowing the HDG file.

0 Kudos
Reply

967 Views
deepaktajanpure
Contributor II

But you have not enabled any chip select in this script. Will you please check it again?

0 Kudos
Reply

1,266 Views
pengyong_zhang
NXP Employee
NXP Employee

hi @deepaktajanpure 

Please choose the default setting of ARM Speed and the attachment file try. 

pengyong_zhang_0-1721613242218.png

B.R

 

0 Kudos
Reply

1,025 Views
deepaktajanpure
Contributor II

Still calibration is failing. Please go through below logs and inc file attached herewith

============================================
        DDR Stress Test (2.4.0) 
        Build: Mar  7 2016, 11:17:32
        Freescale Semiconductor, Inc.
============================================

 

============================================
        Chip ID
CHIP ID = i.MX6 Solo/DualLite (0x61)
Internal Revision = TO1.4
============================================

 

============================================
        Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00008000
SRC_SBMR2(0x020d801c) = 0x21000001
============================================

 

ARM Clock set to 800MHz

 

============================================
        DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is LPDDR2 in 1-channel mode.
Data width: 32, bank num: 4
Row size: 13, col size: 9
Chip select CSD0 is used 
Density per chip select: 64MB 
Density per channel: 64MB 
============================================

 

Current Temperature: 35
============================================

 

DDR Freq: 297 MHz

 

Note: Array result[] holds the DRAM test result of each byte.  
      0: test pass.  1: test fail  
      4 bits respresent the result of 1 byte.    
      result 0001:byte 0 fail. 
      result 0011:byte 0, 1 fail.

 

Starting Read calibration...

 

ABS_OFFSET=0x00000000  result[00]=0x1111
ABS_OFFSET=0x04040404  result[01]=0x1111
ABS_OFFSET=0x08080808  result[02]=0x1111
ABS_OFFSET=0x0C0C0C0C  result[03]=0x1111
ABS_OFFSET=0x10101010  result[04]=0x1111
ABS_OFFSET=0x14141414  result[05]=0x1111
ABS_OFFSET=0x18181818  result[06]=0x0010
ABS_OFFSET=0x1C1C1C1C  result[07]=0x0010
ABS_OFFSET=0x20202020  result[08]=0x0010
ABS_OFFSET=0x24242424  result[09]=0x0010
ABS_OFFSET=0x28282828  result[0A]=0x0010
ABS_OFFSET=0x2C2C2C2C  result[0B]=0x0010
ABS_OFFSET=0x30303030  result[0C]=0x0010
ABS_OFFSET=0x34343434  result[0D]=0x0010
ABS_OFFSET=0x38383838  result[0E]=0x0010
ABS_OFFSET=0x3C3C3C3C  result[0F]=0x0010
ABS_OFFSET=0x40404040  result[10]=0x0010
ABS_OFFSET=0x44444444  result[11]=0x0010
ABS_OFFSET=0x48484848  result[12]=0x0010
ABS_OFFSET=0x4C4C4C4C  result[13]=0x0010
ABS_OFFSET=0x50505050  result[14]=0x0010
ABS_OFFSET=0x54545454  result[15]=0x0010
ABS_OFFSET=0x58585858  result[16]=0x0010
ABS_OFFSET=0x5C5C5C5C  result[17]=0x0010
ABS_OFFSET=0x60606060  result[18]=0x1010
ABS_OFFSET=0x64646464  result[19]=0x1111
ABS_OFFSET=0x68686868  result[1A]=0x1111
ABS_OFFSET=0x6C6C6C6C  result[1B]=0x1111
ABS_OFFSET=0x70707070  result[1C]=0x1111
ABS_OFFSET=0x74747474  result[1D]=0x1111
ABS_OFFSET=0x78787878  result[1E]=0x1111
ABS_OFFSET=0x7C7C7C7C  result[1F]=0x1111

 

Byte 0: (0x18 - 0x60), middle value:0x3c
ERROR FOUND, we can't get suitable value !!!!
dram test fails for all values.

 

Error: failed during ddr calibration

0 Kudos
Reply

1,437 Views
pengyong_zhang
NXP Employee
NXP Employee

hi @deepaktajanpure 

Use the attachment file test again.

0 Kudos
Reply

1,416 Views
deepaktajanpure
Contributor II

Hi

your excel sheet is for imx6sx. Excel sheet version is older v1.1, we are using 1.4. sheet is defined for different LPDDR part number (MT42L256M32D2) ours is MT42L16M32D1HE

0 Kudos
Reply

1,439 Views
pengyong_zhang
NXP Employee
NXP Employee

hi, @deepaktajanpure 

Please share your ddr tool setting windows.

0 Kudos
Reply

1,527 Views
pengyong_zhang
NXP Employee
NXP Employee

HI @deepaktajanpure 

Please use the attachment test.

0 Kudos
Reply

1,515 Views
deepaktajanpure
Contributor II

Hi, executed file sent by you, but still same problem. It is getting stucked in calibration. Please see the logs shown below

============================================
DDR Stress Test (3.0.0)
Build: Dec 14 2018, 14:12:28
NXP Semiconductors.
============================================

============================================
Chip ID
CHIP ID = i.MX6 Solo/DualLite (0x61)
Internal Revision = TO1.4
============================================

============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00008000
SRC_SBMR2(0x020d801c) = 0x21000001
============================================

ARM Clock set to 1GHz

============================================
DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is LPDDR2 in 1-channel mode.
Data width: 32, bank num: 4
Row size: 13, col size: 9
No chip select is enabled
Density per chip select: 64MB
Density per channel: 64MB
============================================

Current Temperature: 49
============================================

DDR Freq: 396 MHz

0 Kudos
Reply

1,586 Views
pengyong_zhang
NXP Employee
NXP Employee

please share your fail log file.

0 Kudos
Reply

1,581 Views
deepaktajanpure
Contributor II

When we click on Calibration it is getting hang. Please see DDR Stress Tester snapshot and log file attached herewith

0 Kudos
Reply

1,612 Views
pengyong_zhang
NXP Employee
NXP Employee

Please use the following setting:

pengyong_zhang_0-1721113576670.png

 

0 Kudos
Reply

1,608 Views
deepaktajanpure
Contributor II

Thanks for your reply. Already done the changes you have mentioned, but still not working. Is there anything left?

0 Kudos
Reply

1,487 Views
pengyong_zhang
NXP Employee
NXP Employee

hi, @deepaktajanpure 

Sure, please share your DDR Datasheet.

B.R

0 Kudos
Reply

1,465 Views
deepaktajanpure
Contributor II

Please find datasheet attached herewith

0 Kudos
Reply