Hi, I want to do LPDDR2 Stress testing on imx6solo custom board. So will you please provide .inc file or any other utility for doing this. DDR Used is MT42L16M32D1HE-18
FIrstly, You do not need to modify the RPA .inc file. Just set the right DDR parameter is OK.
And the RPA file thay i have sened to you is no issue follow your DDR type. So please check your DDR layout is no problem.
B.R
hi, @deepaktajanpure
what do you mean enable chip select? what is your each step?
I just enabled CS0 using below line
setmem /32 0x021b0000 = 0x82010000 // MMDC0_MDCTL
which was not there in your previous script
Hi, @deepaktajanpure
What so you mean not enabled any chip select? you can see the RPA file.
After enabling Chip Select I'm getting same error as I posted below. Calibration fails again
hi, @deepaktajanpure
PLease use the attachment file, And also check your PCB design if is folllowing the HDG file.
But you have not enabled any chip select in this script. Will you please check it again?
Still calibration is failing. Please go through below logs and inc file attached herewith
============================================
DDR Stress Test (2.4.0)
Build: Mar 7 2016, 11:17:32
Freescale Semiconductor, Inc.
============================================
============================================
Chip ID
CHIP ID = i.MX6 Solo/DualLite (0x61)
Internal Revision = TO1.4
============================================
============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00008000
SRC_SBMR2(0x020d801c) = 0x21000001
============================================
ARM Clock set to 800MHz
============================================
DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is LPDDR2 in 1-channel mode.
Data width: 32, bank num: 4
Row size: 13, col size: 9
Chip select CSD0 is used
Density per chip select: 64MB
Density per channel: 64MB
============================================
Current Temperature: 35
============================================
DDR Freq: 297 MHz
Note: Array result[] holds the DRAM test result of each byte.
0: test pass. 1: test fail
4 bits respresent the result of 1 byte.
result 0001:byte 0 fail.
result 0011:byte 0, 1 fail.
Starting Read calibration...
ABS_OFFSET=0x00000000 result[00]=0x1111
ABS_OFFSET=0x04040404 result[01]=0x1111
ABS_OFFSET=0x08080808 result[02]=0x1111
ABS_OFFSET=0x0C0C0C0C result[03]=0x1111
ABS_OFFSET=0x10101010 result[04]=0x1111
ABS_OFFSET=0x14141414 result[05]=0x1111
ABS_OFFSET=0x18181818 result[06]=0x0010
ABS_OFFSET=0x1C1C1C1C result[07]=0x0010
ABS_OFFSET=0x20202020 result[08]=0x0010
ABS_OFFSET=0x24242424 result[09]=0x0010
ABS_OFFSET=0x28282828 result[0A]=0x0010
ABS_OFFSET=0x2C2C2C2C result[0B]=0x0010
ABS_OFFSET=0x30303030 result[0C]=0x0010
ABS_OFFSET=0x34343434 result[0D]=0x0010
ABS_OFFSET=0x38383838 result[0E]=0x0010
ABS_OFFSET=0x3C3C3C3C result[0F]=0x0010
ABS_OFFSET=0x40404040 result[10]=0x0010
ABS_OFFSET=0x44444444 result[11]=0x0010
ABS_OFFSET=0x48484848 result[12]=0x0010
ABS_OFFSET=0x4C4C4C4C result[13]=0x0010
ABS_OFFSET=0x50505050 result[14]=0x0010
ABS_OFFSET=0x54545454 result[15]=0x0010
ABS_OFFSET=0x58585858 result[16]=0x0010
ABS_OFFSET=0x5C5C5C5C result[17]=0x0010
ABS_OFFSET=0x60606060 result[18]=0x1010
ABS_OFFSET=0x64646464 result[19]=0x1111
ABS_OFFSET=0x68686868 result[1A]=0x1111
ABS_OFFSET=0x6C6C6C6C result[1B]=0x1111
ABS_OFFSET=0x70707070 result[1C]=0x1111
ABS_OFFSET=0x74747474 result[1D]=0x1111
ABS_OFFSET=0x78787878 result[1E]=0x1111
ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111
Byte 0: (0x18 - 0x60), middle value:0x3c
ERROR FOUND, we can't get suitable value !!!!
dram test fails for all values.
Error: failed during ddr calibration
Hi
your excel sheet is for imx6sx. Excel sheet version is older v1.1, we are using 1.4. sheet is defined for different LPDDR part number (MT42L256M32D2) ours is MT42L16M32D1HE
hi, @deepaktajanpure
Please share your ddr tool setting windows.
Hi, executed file sent by you, but still same problem. It is getting stucked in calibration. Please see the logs shown below
============================================
DDR Stress Test (3.0.0)
Build: Dec 14 2018, 14:12:28
NXP Semiconductors.
============================================
============================================
Chip ID
CHIP ID = i.MX6 Solo/DualLite (0x61)
Internal Revision = TO1.4
============================================
============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00008000
SRC_SBMR2(0x020d801c) = 0x21000001
============================================
ARM Clock set to 1GHz
============================================
DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is LPDDR2 in 1-channel mode.
Data width: 32, bank num: 4
Row size: 13, col size: 9
No chip select is enabled
Density per chip select: 64MB
Density per channel: 64MB
============================================
Current Temperature: 49
============================================
DDR Freq: 396 MHz
please share your fail log file.
Please use the following setting:
Thanks for your reply. Already done the changes you have mentioned, but still not working. Is there anything left?