imx6sl evk debug led

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6sl evk debug led

2,573件の閲覧回数
eugenephua
Contributor III

Hi there, i am trying to control the debug led on the imx6sl-evk board. I have read posts on it and they have included the debug led support in the linux kernel at linux/imx6sl-evk.dts at master · torvalds/linux · GitHub. However, for the linux kernel at Freescale: linux-2.6-imx.git - Freescale i.MX Linux Tree, the debug led support is not present.

I have tried adding the following in the imx6sl-evk.dts:

leds {

    pinctrl-names = "default";

    pinctrl-0 = <&pinctrl_led>;

    compatible = "gpio-leds";       

   

    user {

        label = "Heartbeat";

        gpios = <&gpio3 20 0>;

        linux,default-trigger = "heartbeat";

    };

};

and in imx6sl.dtsi under iomux:

leds {

        pinctrl_led: ledgrp {

            fsl,pins = <

                MX6SL_PAD_HSIC_STROBE__GPIO3_IO20 0x17059

            >;

        };

    };

But however, i am unable to generate the dtb file. The error is syntax error in the imx6sl-evk.dts file where the "leds" is at. Any advise on this? Thanks!

ラベル(2)
2 返答(返信)

2,010件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Was the last answer helpful?

Best Regards,

Alejandro

0 件の賞賛
返信

2,010件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

I think you can use as reference the below example found in our BSP

leds {

          compatible = "gpio-leds";

          debug-led {

           label = "Heartbeat";

            gpios = <&gpio3 25 0>;

           linux,default-trigger = "heartbeat";

                };

           };

/Alejandro