dear freescale team
i have imx6sabrelite board and want to read device unique ID (OCOTP_CFG0, OCOTP_CFG1).
OCOTP_LOCK_TESTER[1] bit is set to 0 as bellow.
Q1. fuse box is in security block on the block diagram. it could be read in non-secure mode ?
Q2. Can i read OCOTP_CFG0, OCOTP_CFG1 in the linux kernel or u-boot c code with physical address without memtool utility?
Best regards,
Hello,
Please look at the following
How to read i.MX6DQ unique ID.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------