Can some kind person suggest where I'm going wrong?
Whenever I try to switch kernel by adding to my local.conf something like:
PREFERRED_PROVIDER_virtual/kernel = "linux-imx"
PREFERRED_VERSION_virtual/kernel = "3.10.17"
I get a function failed install issue:
make[1]: *** No rule to make target `arch/arm/boot/dts/imx6q-nitrogen6x.dtb'. Stop.
I can see the imx6q-sabrelite.dtb is created, not sure why imx6q-nitrogen6x.dtb is needed.
I've only had success with "linux-boundary" so far but my goal is to use the realtime patches from linux-imx-rt_3.10.17.bb
Can anyone help a noob?
I've tried daisy, master-next and dora branches all with the same problem so I must have missed something obvious.
Thanks in advance,
Mike.
解決済! 解決策の投稿を見る。
Hi Michael,
Sorry for the delayed response.
It appears that you've essentially found the answer yourself. The Freescale kernel trees (linux-imx) do contain some level of support for SABRE Lite, but these are essentially untested and unsupported.
For this reason, we configured the machine 'imx6qsabrelite' to be an alias of 'nitrogen6x' and pointed it at linux-boundary in the machine file.
The only machines directly supported by linux-imx are the Freescale-branded machines in meta-fsl-arm/conf/machine/
meta-fsl-arm/conf/machine at daisy · Freescale/meta-fsl-arm · GitHub
Regards,
Eric
Thanks for the help, just noticed that imx6qsabrelite machine conf uses the nitrogen6x.conf and that board is only supported by linux-boundary.
linux-imx supports imx6qsabrelite but not with the default conf :smileysad:!
To solve this issue I'm using a modified nitrogen6x.conf with the nitrogen6x.dtb removed from KERNEL_DEVICETREE.
Mike.
Is your question already answer?
Yes thank you, I've marked Eric's answer as correct above.
I found a boundary Linux real time branch which I'm currently experimenting with.
Thanks.
Hi Mike,
Note that the previous "-rt" kernel was based on the 3.10.17-beta kernel. I just merged the "-rt" patches onto a new branch (boundary-imx_3.10.17_1.0.0_ga-rt):
https://github.com/boundarydevices/linux-imx6/tree/boundary-imx_3.10.17_1.0.0_ga-rt
Eric, please send a recipe adding it ;-)
Hi Otavio,
I first need to grok what's being done with linux-imx-rt.
That recipe seems to define a new PROVIDER. Is that right?
It also seems to just apply the (presumably updated) "-rt" patches to the same SRCREV, which seems sensible and would prevent the need to download an entirely new kernel to test.
The provider is not need.
Yes, adding the patches makes sense.
Please, let's move this discussion to the mailing list ;-)
Hi Michael,
Sorry for the delayed response.
It appears that you've essentially found the answer yourself. The Freescale kernel trees (linux-imx) do contain some level of support for SABRE Lite, but these are essentially untested and unsupported.
For this reason, we configured the machine 'imx6qsabrelite' to be an alias of 'nitrogen6x' and pointed it at linux-boundary in the machine file.
The only machines directly supported by linux-imx are the Freescale-branded machines in meta-fsl-arm/conf/machine/
meta-fsl-arm/conf/machine at daisy · Freescale/meta-fsl-arm · GitHub
Regards,
Eric
Thank you very much for your help, same day turn around is pretty quick in my book!
Mike.
Part of log.do_install:
make: Leaving directory `/home/mike/fsl-community-daisy-bsp2/build/tmp/work/imx6qsabrelite-poky-linux-gnueabi/linux-imx/3.10.17-r0/image/usr/src/kernel'
| NOTE: make -j 8 imx6q-sabrelite.dtb
| CC scripts/mod/devicetable-offsets.s
| GEN scripts/mod/devicetable-offsets.h
| HOSTCC scripts/mod/file2alias.o
| HOSTLD scripts/mod/modpost
| DTC arch/arm/boot/dts/imx6q-sabrelite.dtb
| NOTE: make -j 8 imx6q-nitrogen6x.dtb
| CC scripts/mod/devicetable-offsets.s
| GEN scripts/mod/devicetable-offsets.h
| HOSTCC scripts/mod/file2alias.o
| HOSTLD scripts/mod/modpost
| make[1]: *** No rule to make target `arch/arm/boot/dts/imx6q-nitrogen6x.dtb'. Stop.
| make: *** [imx6q-nitrogen6x.dtb] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_install (log file is located at /home/mike/fsl-community-daisy-bsp2/build/tmp/work/imx6qsabrelite-poky-linux-gnueabi/linux-imx/3.10.17-r0/temp/log.do_install.22321)
ERROR: Task 2 (/home/mike/fsl-community-daisy-bsp2/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb, do_install) failed with exit code '1'
you may check what bitbake is doing with
bitbake -c install -f -e linux-imx
?
I think the PREFERED_VERSION needs the PN also, so you can try
PREFERRED_VERSION_virtual/kernel_linux-imx = "3.10.17"
Sorry my mistake above in the example I would have used PREFERRED_VERSION_linux_imx = "3.10.17"
I'm still seeing the same issue.