imx6qdlsabresd: USB OTG issue with u-boot-imx 2022.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6qdlsabresd: USB OTG issue with u-boot-imx 2022.04

1,508 Views
SebastienFabre
Contributor II

I am working on imx6qdlsabresd on yocto kirstone.

When using u-boot-imx (2022.04), I have some issues with usb otg. If I connect a mouse to the USB OTG port, after moving it several seconds (less than 1 minute), no more event is sent (can be seen with evtest tool) and the port is reset (after several seconds).

[ 44.546052] usb 2-1: new low-speed USB device number 3 using ci_hdrc
[ 44.752376] usb 2-1: New USB device found, idVendor=093a, idProduct=2510, bcdDevice= 1.00
[ 44.760745] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 44.768014] usb 2-1: Product: USB Optical Mouse
[ 44.772580] usb 2-1: Manufacturer: PixArt
[ 44.783470] input: PixArt USB Optical Mouse as /devices/platform/soc/2100000.bus/2184000.usb/ci_hdrc.0/usb2/2-1/2-1:1.0/0003:093A:2510.0002/input/input8
[ 44.797440] hid-generic 0003:093A:2510.0002: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-ci_hdrc.0-1/input0
[ 107.516305] random: crng init done
[ 107.519743] random: 2 urandom warning(s) missed due to ratelimiting
[ 124.468579] usb 2-1: USB disconnect, device number 3
[ 126.006006] usb 2-1: new low-speed USB device number 4 using ci_hdrc
[ 126.212860] usb 2-1: New USB device found, idVendor=093a, idProduct=2510, bcdDevice= 1.00
[ 126.221146] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 126.228384] usb 2-1: Product: USB Optical Mouse
[ 126.232946] usb 2-1: Manufacturer: PixArt
[ 126.243987] input: PixArt USB Optical Mouse as /devices/platform/soc/2100000.bus/2184000.usb/ci_hdrc.0/usb2/2-1/2-1:1.0/0003:093A:2510.0003/input/input9
[ 126.257914] hid-generic 0003:093A:2510.0003: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-ci_hdrc.0-1/input0

Moreover, sometimes, several seconds (less than 1 minute) after connecting usb stick (no mount performed), the port is reset.

[ 170.476078] usb 2-1: new high-speed USB device number 5 using ci_hdrc
[ 170.678240] usb 2-1: New USB device found, idVendor=21c4, idProduct=0cd1, bcdDevice=11.00
[ 170.686520] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 170.693721] usb 2-1: Product: USB Flash Drive
[ 170.698150] usb 2-1: Manufacturer: Lexar
[ 170.702098] usb 2-1: SerialNumber: 04PAH98A4QFYZNI9
[ 170.709168] usb-storage 2-1:1.0: USB Mass Storage device detected
[ 170.715847] scsi host1: usb-storage 2-1:1.0
[ 171.931658] scsi 1:0:0:0: Direct-Access Lexar USB Flash Drive 1100 PQ: 0 ANSI: 6
[ 171.943602] sd 1:0:0:0: [sda] 60620800 512-byte logical blocks: (31.0 GB/28.9 GiB)
[ 171.953197] sd 1:0:0:0: [sda] Write Protect is off
[ 171.958051] sd 1:0:0:0: [sda] Mode Sense: 43 00 00 00
[ 171.959240] sd 1:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
[ 171.976420] sda: sda1
[ 171.983504] sd 1:0:0:0: [sda] Attached SCSI removable disk
[ 202.246029] usb 2-1: reset high-speed USB device number 5 using ci_hdrc
[ 202.447734] sd 1:0:0:0: [sda] tag#0 FAILED Result: hostbyte=DID_TIME_OUT driverbyte=DRIVER_OK cmd_age=30s
[ 202.457408] sd 1:0:0:0: [sda] tag#0 CDB: Read(10) 28 00 03 9c ff fe 00 00 01 00
[ 202.464743] blk_update_request: I/O error, dev sda, sector 60620798 op 0x0:(READ) flags 0x80700 phys_seg 1 prio class 0

[ 232.966052] usb 2-1: reset high-speed USB device number 5 using ci_hdrc
[ 233.167575] sd 1:0:0:0: [sda] tag#0 FAILED Result: hostbyte=DID_TIME_OUT driverbyte=DRIVER_OK cmd_age=30s
[ 233.177366] sd 1:0:0:0: [sda] tag#0 CDB: Read(10) 28 00 00 00 00 28 00 00 10 00
[ 233.184743] blk_update_request: I/O error, dev sda, sector 40 op 0x0:(READ) flags 0x80700 phys_seg 2 prio class 0
[ 233.943246] udevd[172]: worker [412] /devices/platform/soc/2100000.bus/2184000.usb/ci_hdrc.0/usb2/2-1/2-1:1.0/host1/target1:0:0/1:0:0:0/block/sda is taking a long time

...

I have these issues with linux-imx or linux-fslc-imx.

It seems that I do not have these issues with u-boot-fslc (2022.10).

 

I have also additional issues:

0 Kudos
Reply
10 Replies

1,485 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @SebastienFabre 

I hope you are doing well.

One of the possible cause of USB reset is power fluctuation of USB. Can you please check the USB VBUS power rails while you see the reset logs?

Thanks & Regards

Sanket Parekh

0 Kudos
Reply

1,473 Views
SebastienFabre
Contributor II

Hello,

Even when I see reset log, USB VBUS stays equal to 5V.

Moreover, about issue on u-boot-fslc 2022.10 to detect sdcard, we can update:

- arch/arm/dts/imx6qdl-sabresd.dtsi with

aliases {
mmc1 = &usdhc3;
};

- arch/arm/dts/imx6qdl-wandboard.dtsi with

aliases {
mmc0 = &usdhc3;
};

Best regards

 

 

 

0 Kudos
Reply

1,463 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @SebastienFabre 

Can you please share your board DTS files?

Thanks & Regards

Sanket Parekh

0 Kudos
Reply

1,453 Views
SebastienFabre
Contributor II

Hello,

As said before I am using yocto kirkstone. You can reproduce this issue with yocto kirkstone imx manifest (repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.32-2.0.0.xml), MACHINE equals to imx6qdlsabresd, DISTRO equal to fsl-imx-xwayland (I think that we have the same issue with other distros) and with core-image-weston image (I think that we have the same issue with other images).

As said before, the issue seems to not be reproduced with u-boot-fslc (IMX_DEFAULT_BOOTLOADER:imx-nxp-bsp = "u-boot-fslc" in local.conf +  PREFERRED_PROVIDER_virtual/bootloader:imx-nxp-bsp = "u-boot-fslc" in fsl-imx-preferred-env.inc)

Best regards

0 Kudos
Reply

1,434 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @SebastienFabre 

I hope you are doing well
 
Thanks for your patience.
 
We tried to reproduce the issue on yocto kirkstone imx manifest with BSP version 5.15.32 on the IMX8MQ and IMX8MP board as we have no imx6qdlsabresd board setup. But the USB device works fine on our end. We kindly recommend you please cross-varify your hardware. It seems that the issue is not from the BSP side.
 
Thanks & Regards
Sanket Parekh
0 Kudos
Reply

1,424 Views
SebastienFabre
Contributor II

Hello,

On the same board, there is the issue in case of u-boot-imx whereas it is OK in case of u-boot-fslc. I have the same behavior with another imx6qdlsabresd board. So it should not be an hardware issue.

I think there is an issue in u-boot-imx (code or device tree) at least for imx6qdlsabresd board. I have not tested with other imx6 boards.

Best regards

Sébastien

0 Kudos
Reply

1,399 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
We confirmed that there is no issue on iMX8 with the same version of u-boot-imx (2022.04) and we are trying for the same setup of imx6qdlsabresd.
We are working on that. We will get back to you soon.
 
Thanks & Regards
Sanket Parekh
0 Kudos
Reply

1,393 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @SebastienFabre 

I really appreciate your patience.
We tried the same setup as you have with the imx6qdlsabresd board with the same BSP you mentioned.
But we failed to reproduce the issue on our end and the mouse connected with OTG is being detected, also port is not getting reset.
We observed this scenario for more than half an hour but the result is the same.
 
Thanks & Regards
Sanket Parekh
 

0 Kudos
Reply

1,364 Views
SebastienFabre
Contributor II

Hello,

So, when you use u-boot-imx (2022.04) with kirkstone on imx6qdlsabresd, if you connect your mouse on USB OTG port, it is always detected even if you move it several seconds or minutes (less than 5) ?

If so, I don't understand why I can reproduce the issue on 2 boards with u-boot-imx (2022.04) and not with u-boot-fslc (2022.10)

Best regards

0 Kudos
Reply

1,342 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @SebastienFabre 

So, when you use u-boot-imx (2022.04) with kirkstone on imx6qdlsabresd, if you connect your mouse on USB OTG port, it is always detected even if you move it several seconds or minutes (less than 5) ?

=> Yes
 
If so, I don't understand why I can reproduce the issue on 2 boards with u-boot-imx (2022.04) and not with u-boot-fslc (2022.10)
=> I have sent this issue to our engineering team. We will get back to you as soon as we get any clue.
 
Thanks & Regards
Sanket Parekh

0 Kudos
Reply