大家好:
我现在给我们板子移植bcm43341 wifi驱动,现在可以ping通手机热点。android的界面打开wifi开关
屏上可以看到搜索周围的热点但是连接的时候,终端打印如下错误:
[ 205.827209] Connectting with 6a:3e:34:03:0b:00 channel (2) ssid "QYAP-V2-23456-m2 note-fd", len (24)
[ 205.935793] wl_iw_event: Link UP with BSSID=6A:3E:00:00:0B:00
[ 205.942046] wl_bss_connect_done succeeded with 6a:3e:34:03:0b:00
[ 206.066152] dhd_pno_get_for_batch : wifi location service is not supported
[ 206.073382] CFG80211-ERROR) wl_is_linkdown :
[ 206.077726] ANDROID-ERROR) failed to getting batching results
[ 206.083883] Link down Reason : WLC_E_DEAUTH_IND
[ 206.088643] link down if eth1 may call cfg80211_disconnected. event : 6, reason=3 from 6a:3e:34:03:0b:00
[ 206.090870] dhd_pno_stop_for_batch : wifi location service is not supported
[ 206.090880] NULL POINTER (_dhd_pno_clear_all_batch_results) : head->next is NULL
[ 206.090887] NULL POINTER (_dhd_pno_clear_all_batch_results) : head->next is NULL
[ 206.090893] ANDROID-ERROR) failed to stop batching scan
[ 206.127908] wl_iw_event: Link Down with BSSID=6A:3E:00:00:0B:00
[ 206.134411] CFG80211-ERROR) wl_is_linkdown : Link down Reason : WLC_E_LINK
[ 206.143106] cfg80211: Calling CRDA to update world regulatory domain
[ 206.904686] p2p0: no IPv6 routers present
[ 207.704866] Connectting with 6a:3e:34:03:0b:00 channel (2) ssid "QYAP-V2-23456-m2 note-fd", len (24)
[ 208.695265] connect failed event=0 e->status 3 e->reason 0
[ 208.704249] CFG80211-ERROR) wl_bss_connect_done : Report connect result - connection failed
android上层打印的错误如下:
dhcp_do_request failed :eth1(new)
DHCP request error:Timed out waiting for DHCP to finish
现在主要是我手动
1、加载驱动
2、启动网卡(报个错:dhd_preinit_ioctls wl ampdu_hostreorder failed -23)
3、扫描周围热点
4、通过udhcp获取ip,ping手机成功
android 的界面上可以打开wifi开关,可以扫描到周围热点,但是连接的时候就一直报上面的错误。
问题早解决
在 2018-06-22 16:33:35,"赵振业" <admin@community.nxp.com> 写道:
|
|
NXP Community
|
|
Re: imx6qQ 移植ap6441(bcm43341 wifi)
reply from 赵 振业 in i.MX Community - View the full discussion
问题解决了么
Reply to this message by replying to this email, or go to the message on NXP Community |
Start a new discussion in i.MX Community by email or at NXP Community |
Following Re: imx6qQ 移植ap6441(bcm43341 wifi) in these streams: Inbox |
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences
|
|
是因为厂家的给的驱动包不是最新的造成的,最后厂家更新了一个驱动包,问题解决。
在 2019-03-14 15:06:16,"wangtsungli" <admin@community.nxp.com> 写道:
|
|
NXP Community
|
|
Re: imx6qQ 移植ap6441(bcm43341 wifi)
reply from tsung li wang in i.MX Processors - View the full discussion
請問你是如何解決的呢?
我在 ubuntu 16.04 lxde 上面用 networkmanager 連接wifi 也遇到一樣的問題。
Reply to this message by replying to this email, or go to the message on NXP Community |
Start a new discussion in i.MX Processors by email or at NXP Community |
Following Re: imx6qQ 移植ap6441(bcm43341 wifi) in these streams: Inbox |
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences
|
|
上层的打印
/wpa_supplicant( 3390): eth1: Associated with 28:6c:07:56:f9:25
D/Ethernet( 2642): Interface eth1 link up
D/Ethernet( 2642): Interface eth1 link up
D/Ethernet( 2642): Interface eth1 link up
D/Ethernet( 2642): Interface eth1 link up
D/Ethernet( 2642): Interface eth1 link up
I/wpa_supplicant( 3390): eth1: WPA: Key negotiation completed with 28:6c:07:56:f9:25 [PTK=CCMP GTK=TKIP]
I/wpa_supplicant( 3390): eth1: CTRL-EVENT-CONNECTED - Connection to 28:6c:07:56:f9:25 completed (auth) [id=0 id_str=]
D/Ethernet( 2642): Interface eth1 link up
E/wpa_supplicant( 3390): wpa_driver_nl80211_driver_cmd: failed to issue private commands
E/WifiStateMachine( 2642): Unexpected BatchedScanResults :null
E/wpa_supplicant( 3390): wpa_driver_nl80211_driver_cmd: failed to issue private commands
I/wpa_supplicant( 3390): eth1: WPA: Key negotiation completed with 28:6c:07:56:f9:25 [PTK=CCMP GTK=TKIP]
D/WifiStateMachine( 2642): VerifyingLinkState enter
D/WifiStateMachine( 2642): VerifyingLinkState GOOD_LINK_DETECTED: transition to captive portal check
D/WifiStateMachine( 2642): CaptivePortalCheckState enter
D/WifiStateMachine( 2642): CaptivePortalCheckState CMD_CAPTIVE_CHECK_COMPLETE
D/ConnectivityService( 2642): Captive portal check NetworkInfo: type: WIFI[], state: CONNECTING/CAPTIVE_PORTAL_CHECK, reason: (unspecified), extra: "lovensMIWIFI", roaming: false, failover: false, isAvailable: true, isConnectedToProvisioningNetwork: false
D/ConnectivityService( 2642): handleCaptivePortalTrackerCheck: call captivePortalCheckComplete ni=NetworkInfo: type: WIFI[], state: CONNECTING/CAPTIVE_PORTAL_CHECK, reason: (unspecified), extra: "lovensMIWIFI", roaming: false, failover: false, isAvailable: true, isConnectedToProvisioningNetwork: false
D/ConnectivityService( 2642): ConnectivityChange for WIFI: CONNECTED/CONNECTED
E/ConnectivityService( 2642): Unexpected mtu value: android.net.wifi.WifiStateTracker@41965b70
D/Nat464Xlat( 2642): requiresClat: netType=1, hasIPv4Address=true
D/ConnectivityService( 2642): ConnectivityChange for ETHERNET: CONNECTED/CONNECTED
D/ConnectivityService( 2642): Policy requires WIFI teardown
I/wpa_supplicant( 3390): eth1: CTRL-EVENT-DISCONNECTED bssid=28:6c:07:56:f9:25 reason=3 locally_generated=1
E/ConnectivityService( 2642): Unexpected mtu value: android.net.EthernetDataTracker@41ae41d0
D/Ethernet( 2642): Interface eth1 link up
D/NetUtils( 2642): dhcp_do_request failed : eth1 (new)
E/Ethernet( 2642): DHCP request error:Timed out waiting for DHCP to finish
Hi xiaoliang
one can check android guide
wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_android.pdf
and request additional help on vendor support
wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------