imx6q with ksz8795 ethernet transmission abnormal stop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q with ksz8795 ethernet transmission abnormal stop

553 Views
qq8341248
Contributor I

board: designed by us refer to sabreLite-D
cpu: imx6q(MCIMX6Q6AVT10AD)
net switches: ksz8795(1 rgmii interface,4 10/100Mbps ports)
net interface: rgmii 1000Mbps
imx6q ENET_REF_CLK: from FPGA dedicated PLL clk output pin
memory device: emmc 4.4.1
ftp tools: FlashFXP

transceiving mode(rgmii):
up link: emmc to pc
down link: pc to emmc

switch function(phy):
port 1 to port 2


we use imx6q and ksz8795 (datasheet in KSZ8795 - Interface and Networking - Ethernet Switches - Microcontrollers and Processors ) as ethernet partner, the ksz8795's switch function is nomal when we make a 4GB file transceiving deal by FlashFXP between them. however when we use rgmii to transceiving 4GB file by FlashFXP,we find the transceiving encounter several abnormal stops(sometimes the transceiving is normal,sometimes it's abnormal, the transceiving seems to be unstable ), we print all register when the deal is in the normal transceiving (normal mode)and when the deal is stop (abnormal mode),someuseful information is as below.

 

1. in one deal there are phenomenons like this:
1.1 up link
normal mode : 
imx6 register : 0x02188004 = 0x00000000(TXF=0 TXB=0 RXF=0), 0x02188008 = 0x2c000000(BABT=0 RXF=0 RXB=0)
phy register : 0x1e = 60(MDIX status= MDI-X)

 

abnormal mode : 
imx6 register : 0x02188004 = 0x0e000000(TXF=1 TXB=1 RXF=1), 0x02188008 = 0x6f000000(BABT=1 RXF=1 RXB=1)
phy register : 0x1e = e0(MDIX status= MDI)

 

in this situation, when transceiving is stop, ksz8795 seems to make a MDI/MDI-X Auto-Negotiation,but we do 
not change the transceiving environment, in additon ,we cannot understand why imx6q register have such
changes?


2. in another deal there are phenomenons like this:
2.1 up link
normal mode : 
imx6 register : 0x02188004 = 0x00000000(TXF=0 TXB=0 RXF=0), 0x02188008 = 0x2c000000(BABT=0 RXF=0 RXB=0)
0x02188010 = 0x01000000(RADR=1), 0x02188014 = 0x01000000(TDAR=1)
phy register : no change

 

abnormal mode : 
imx6 register : 0x02188004 = 0x0e000000(TXF=1 TXB=1 RXF=1), 0x02188008 = 0x6f000000(BABT=1 RXF=1 RXB=1)
0x02188010 = 0x00000000(RADR=0), 0x02188014 = 0x00000000(TDAR=0)
phy register : no change

 

in this situation,we cannot understand why imx6q register have such changes?


what can i do? which is abnormal? where is abnormal?
urgent waiting for your reply, thanks.

Labels (1)
0 Kudos
1 Reply

425 Views
igorpadykov
NXP Employee
NXP Employee

Hi  杰 王

sbarelite board and its software is supported by its vendor boundary devices,

so issue may be posted to its forum:

Boundary Devices Launches Wiki Page - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos