Hello!
I use imx6q on Sabre SD board with linux 3.14. When I run camera preview via GStreamer or v4l2 itself, after suspend/resume video freezes and "ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0" appears in console.
It seems that IPU resumes incorrect and CSI/IDMA channel resets on suspend and not configures again (IPU tasks are always wait for signal and do nothing).
What should I do to proper resume IPU? May be there are some patches or newer mxc_v4l2_capture or IPU drivers?
in attachement - dmesg output after suspend/resume
-------------------------
EDIT:
It seems that I resolve my question. The algorithm is:
- disable SCI on suspend
- restart stream on resume:
- if ready_q is empty get back one buffer from working_q
- if after that in ready_q only one buffer - get dummy_frame.buffer for "ping-pong"
I added "mxc_streamrestart" function for this purpose. You can get it from patch below. Hope, this patch will not damage anything .
Original Attachment has been moved to: dmesg.log.zip
Original Attachment has been moved to: 0001-fix-camera-preview-fault-after-system-suspend.patch.zip
Hello,
I think i have the same issue . (https://community.nxp.com/t5/i-MX-Processors/Error-on-standby-mode-due-to-gstreamer/m-p/1568373/high...
do you figure it out how to restart stream properly after suspend ?
Best regards
another "internal" source of buffers is working_q. I think I can get buffer back to ready_q from working_q because dma was stopped and data in "working" buffer are useless. But what if working_q will be empty too? Is it real in suspend/resume case? Can I get buffers from cam->frame array by the driver without signalling to userspace?
It seems I found way to restart IDMA channel after suspend/resume:
- call cam->enc_disable_csi(cam); on suspend to clear irq handlers and reset ipu->csi_use_count. It is needed to start IDMA flow on resume with standard IPU API;
- do cam->capture_on = false; before mxc_streamon(cam); on resume to start stream. Else if cam->capture_on == true, mxc_streamon do nothing.
BUT there is one problem: I haven't enough buffers in ready_q queue after resume and stream can't start because "mxc_streamon buffer need ping pong at least two buffers".
So the question is: Where can I find one more free buffer after resume?