imx6q hanged when boot up the kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q hanged when boot up the kernel

725件の閲覧回数
逍遥李
Contributor II

1.environment :

         CPU: imx6q 1.2Ghz

         DDR: 4GB

         EMMC: 32GB

2.bug:

         1) after Starting kernel... the program hanged, uart log as the attachment.

         2) I found the program hanged at the function "of_clk_init(NULL)" (kernel/arch/arm/mach-imx/Mach-imx6q.c imx6q_timer_init() );

Could you please help me fix the problem???

ラベル(2)
タグ(3)
0 件の賞賛
2 返答(返信)

573件の閲覧回数
art
NXP Employee
NXP Employee

The most likely cause of the issue is some inappropriate design of the DDR memory interface, causing it to hang when switching to higher operational frequency. Please check your DDR interface design according to the Sections 3.1 to 3.6 of the i.MX6 series Hardware Development Guide document, available on the processor's Documentation web page:

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/arm-mcus-and-mpus/i....

Pay the special attention to the traces impedance matching as per the Section 3.3 and trace length matching as per the Section 3.4.

Also, check the set points of the VDD_ARM_CAP, VDD_SOC_CAP and VDD_PU_CAP power rails, they should be between 1.25V and 1.3V for 1.2GHz operatin


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

573件の閲覧回数
逍遥李
Contributor II

Dear all,

            my base is android_L5.0, I have changed the .dtb file to cancle the bypass mode. Is there any others need to modified??????

             I haved changed all the "fsl, ldo-bypass" node, as follow, and make the imx6q-sabresd-ldo.dtb in device tree.

                        fsl,ldo-bypass = <1>——>fsl,ldo-bypass = <0>

0 件の賞賛