My custom board: reference mx6q_sabreauto BSP: 4.1.15_1.0.0_ga , I can use mfg boot uboot ,but I use sd boot form uSDHC4 and ecspi1,but it not success ,we use ddr test tool create new calibration settings and rebuild uboot
============================================
DDR Stress Test (2.5.2)
Build: Mar 31 2016, 23:07:26
Freescale Semiconductor, Inc.
============================================
============================================
Chip ID
CHIP ID = i.MX6 Dual/Quad (0x63)
Internal Revision = TO1.5
============================================
============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00000001
SRC_SBMR2(0x020d801c) = 0x31000001
============================================
ARM Clock set to 1GHz
============================================
DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3
Data width: 32, bank num: 8
Row size: 15, col size: 10
Chip select CSD0 is used
Density per chip select: 1024MB
============================================
Current Temperature: 53
============================================
DDR Freq: 297 MHz
ddr_mr1=0x00000000
Start write leveling calibration...
running Write level HW calibration
Write leveling calibration completed, update the following registers in your initialization script
MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x001F0023
MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x002B001F
Write DQS delay result:
Write DQS0 delay: 35/256 CK
Write DQS1 delay: 31/256 CK
Write DQS2 delay: 31/256 CK
Write DQS3 delay: 43/256 CK
WARNING: write-leveling calibration value is greater than 1/8 CK.
Per the reference manual, WALAT must be set to 1 in the register MDMISC(0x021B0018).
This has been performed automatically.
However, in addition to updating the calibration values in your DDR initialization,
it is also REQUIRED change the value of MDMISC in their DDR initialization as follows:
MMDC_MDMISC (0x021b0018) = 0x00011740
Starting DQS gating calibration
. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .
. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .
BYTE 0:
Start: HC=0x01 ABS=0x00
End: HC=0x02 ABS=0x5C
Mean: HC=0x01 ABS=0x6D
End-0.5*tCK: HC=0x01 ABS=0x5C
Final: HC=0x01 ABS=0x6D
BYTE 1:
Start: HC=0x00 ABS=0x78
End: HC=0x02 ABS=0x54
Mean: HC=0x01 ABS=0x66
End-0.5*tCK: HC=0x01 ABS=0x54
Final: HC=0x01 ABS=0x66
BYTE 2:
Start: HC=0x01 ABS=0x00
End: HC=0x02 ABS=0x58
Mean: HC=0x01 ABS=0x6B
End-0.5*tCK: HC=0x01 ABS=0x58
Final: HC=0x01 ABS=0x6B
BYTE 3:
Start: HC=0x01 ABS=0x00
End: HC=0x02 ABS=0x5C
Mean: HC=0x01 ABS=0x6D
End-0.5*tCK: HC=0x01 ABS=0x5C
Final: HC=0x01 ABS=0x6D
DQS calibration MMDC0 MPDGCTRL0 = 0x4166016D, MPDGCTRL1 = 0x016D016B
Note: Array result[] holds the DRAM test result of each byte.
0: test pass. 1: test fail
4 bits respresent the result of 1 byte.
result 0001:byte 0 fail.
result 0011:byte 0, 1 fail.
Starting Read calibration...
ABS_OFFSET=0x00000000 result[00]=0x1111
ABS_OFFSET=0x04040404 result[01]=0x1111
ABS_OFFSET=0x08080808 result[02]=0x1011
ABS_OFFSET=0x0C0C0C0C result[03]=0x1000
ABS_OFFSET=0x10101010 result[04]=0x0000
ABS_OFFSET=0x14141414 result[05]=0x0000
ABS_OFFSET=0x18181818 result[06]=0x0000
ABS_OFFSET=0x1C1C1C1C result[07]=0x0000
ABS_OFFSET=0x20202020 result[08]=0x0000
ABS_OFFSET=0x24242424 result[09]=0x0000
ABS_OFFSET=0x28282828 result[0A]=0x0000
ABS_OFFSET=0x2C2C2C2C result[0B]=0x0000
ABS_OFFSET=0x30303030 result[0C]=0x0000
ABS_OFFSET=0x34343434 result[0D]=0x0000
ABS_OFFSET=0x38383838 result[0E]=0x0000
ABS_OFFSET=0x3C3C3C3C result[0F]=0x0000
ABS_OFFSET=0x40404040 result[10]=0x0000
ABS_OFFSET=0x44444444 result[11]=0x0000
ABS_OFFSET=0x48484848 result[12]=0x0000
ABS_OFFSET=0x4C4C4C4C result[13]=0x0100
ABS_OFFSET=0x50505050 result[14]=0x0111
ABS_OFFSET=0x54545454 result[15]=0x1111
ABS_OFFSET=0x58585858 result[16]=0x1111
ABS_OFFSET=0x5C5C5C5C result[17]=0x1111
ABS_OFFSET=0x60606060 result[18]=0x1111
ABS_OFFSET=0x64646464 result[19]=0x1111
ABS_OFFSET=0x68686868 result[1A]=0x1111
ABS_OFFSET=0x6C6C6C6C result[1B]=0x1111
ABS_OFFSET=0x70707070 result[1C]=0x1111
ABS_OFFSET=0x74747474 result[1D]=0x1111
ABS_OFFSET=0x78787878 result[1E]=0x1111
ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111
Byte 0: (0x0c - 0x4c), middle value:0x2c
Byte 1: (0x0c - 0x4c), middle value:0x2c
Byte 2: (0x08 - 0x48), middle value:0x28
Byte 3: (0x10 - 0x50), middle value:0x30
MMDC0 MPRDDLCTL = 0x30282C2C
Starting Write calibration...
ABS_OFFSET=0x00000000 result[00]=0x1111
ABS_OFFSET=0x04040404 result[01]=0x1110
ABS_OFFSET=0x08080808 result[02]=0x0000
ABS_OFFSET=0x0C0C0C0C result[03]=0x0000
ABS_OFFSET=0x10101010 result[04]=0x0000
ABS_OFFSET=0x14141414 result[05]=0x0000
ABS_OFFSET=0x18181818 result[06]=0x0000
ABS_OFFSET=0x1C1C1C1C result[07]=0x0000
ABS_OFFSET=0x20202020 result[08]=0x0000
ABS_OFFSET=0x24242424 result[09]=0x0000
ABS_OFFSET=0x28282828 result[0A]=0x0000
ABS_OFFSET=0x2C2C2C2C result[0B]=0x0000
ABS_OFFSET=0x30303030 result[0C]=0x0000
ABS_OFFSET=0x34343434 result[0D]=0x0000
ABS_OFFSET=0x38383838 result[0E]=0x0000
ABS_OFFSET=0x3C3C3C3C result[0F]=0x0000
ABS_OFFSET=0x40404040 result[10]=0x0000
ABS_OFFSET=0x44444444 result[11]=0x0000
ABS_OFFSET=0x48484848 result[12]=0x0000
ABS_OFFSET=0x4C4C4C4C result[13]=0x0001
ABS_OFFSET=0x50505050 result[14]=0x1101
ABS_OFFSET=0x54545454 result[15]=0x1111
ABS_OFFSET=0x58585858 result[16]=0x1111
ABS_OFFSET=0x5C5C5C5C result[17]=0x1111
ABS_OFFSET=0x60606060 result[18]=0x1111
ABS_OFFSET=0x64646464 result[19]=0x1111
ABS_OFFSET=0x68686868 result[1A]=0x1111
ABS_OFFSET=0x6C6C6C6C result[1B]=0x1111
ABS_OFFSET=0x70707070 result[1C]=0x1111
ABS_OFFSET=0x74747474 result[1D]=0x1111
ABS_OFFSET=0x78787878 result[1E]=0x1111
ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111
Byte 0: (0x04 - 0x48), middle value:0x26
Byte 1: (0x08 - 0x50), middle value:0x2c
Byte 2: (0x08 - 0x4c), middle value:0x2a
Byte 3: (0x08 - 0x4c), middle value:0x2a
MMDC0 MPWRDLCTL = 0x2A2A2C26
MMDC registers updated from calibration
Write leveling calibration
MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x001F0023
MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x002B001F
Read DQS Gating calibration
MPDGCTRL0 PHY0 (0x021b083c) = 0x4166016D
MPDGCTRL1 PHY0 (0x021b0840) = 0x016D016B
Read calibration
MPRDDLCTL PHY0 (0x021b0848) = 0x30282C2C
Write calibration
MPWRDLCTL PHY0 (0x021b0850) = 0x2A2A2C26
Success: DDR calibration completed!!!
use the rebuild u-boot .imx ,can boot from mfgtool in windows pc
U-Boot 2015.04-14468-gd7d7c43-dirty (Aug 24 2016 - 09:59:41)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 42 C
Reset cause: POR
Board: MX6Q-GWI-SCANNER revA
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: MMC/SD: Reset never completed.
voltage not supported by controller
SF: Unsupported flash IDs: manuf 00, jedec 0000, ext_jedec 0000
*** Warning - spi_flash_probe() failed, using default environment
In: serial
Out: serial
Err: serial
Net: Phy 0 not found
PHY reset timed out
FEC [PRIME]
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Bad Linux ARM zImage magic!
=> md 020d8004 1
020d8004: 00003840 @8..
=> md 020d801c 1
020d801c: 30000011 ...0
=>
but I can not boot from sd4 or spinor ,when I insert sd in sd4 , we measuring the signal of SD4_CLK In the annex
Hi xuhui
one can to program sd card with another option, please refer to
attached Linux Guide sect.4.3.1 Preparing the card.
If it fails please attach jtag and check SRC_SBMR1,2
they should contain correct boot settings.
What reference design is based custom board, is it i.MX6Q Sabre SD
or other board?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
you can see my board is reference design imx6q-sabread-AI ,in uboot-imx is mx6qsabreauto,and I use mfgtool boot the board can see SRC_SBMR1,2 :
=> md 020d8004 1
020d8004: 00003840 @8..
=> md 020d801c 1
020d801c: 30000011 ...0
=>
one can attach the board with any JTAG debugger and dump 0x907400
(ROM uses 0x907000 as starting address), you should see your IVT header
here if the SD access is ok. Example can be found on