imx6q custom board stucks at penguins logo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q custom board stucks at penguins logo

487件の閲覧回数
laulavanya
Contributor II

Hi,

Currently display stuck at penguins ,

Using the custom board , for more information please check the logs attached below.

I am suspecting below error

libprocessgroup: Successfully killed process cgroup uid 0 pid 14910 in 110ms
init: Command 'restart zygote' action=onrestart (<Service 'surfaceflinger' onrestart>:1) took 138ms and succeeded
init: Service 'zygote' (pid 14910) received signal 9
init: Command 'write /sys/power/state on' action=onrestart (<Service 'zygote' onrestart>:2) took 0ms and failed: Unable to write to file '/sys/power/state': Unable to write file contents: Invalid argument
init: Sending signal 9 to service 'audioserver' (pid 14911) process group...
libprocessgroup: Successfully killed process cgroup uid 1041 pid 14911 in 10ms

ラベル(4)
0 件の賞賛
返信
0 返答(返信)