imx6q boot issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q boot issue

929 Views
lixuhui112
Contributor I

My custom board: reference mx6q_sabreauto  BSP: 4.1.15_1.0.0_ga , I can use mfg boot uboot ,but I use sd boot form uSDHC4 ,it is not work  ,

Bootmode[1:0]   to 10  boot form boart seting

and sw[8-1] to   0100 0011

but it is not work ,

If  there any need to be configured ,please help me ,

Thanks,

pastedImage_0.png

Labels (1)
0 Kudos
Reply
3 Replies

850 Views
lixuhui112
Contributor I

and I use

Bootmode[1:0]   to 10  boot form boart seting

and sw[8-1] to   00111100

boot form spinor  it also not work

0 Kudos
Reply

850 Views
igorpadykov
NXP Employee
NXP Employee

Hi xuhui

for new board it is necessary to run ddr test and find new calibration

settings, change uboot ../mx6sabresd/mx6q_4x_mt41j128.cfg with new

settings and rebuild uboot

i.MX6/7 DDR Stress Test Tool V2.52 | NXP Community

If board still not boots, attach jtag and check boot settings in register

SRC_SBMR1,2. Also please check Chapter 8 Avoiding Board Bring-up Problems

i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

850 Views
lixuhui112
Contributor I

Hi igor,

Thanks for your reply

my board  can boot use mfgtool  ,  but can not sd and spinor,

0 Kudos
Reply