imx6q NAND: gpmi_reset_block(00112000): module reset timeout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q NAND: gpmi_reset_block(00112000): module reset timeout

482 次查看
haiy
Contributor I

Temperature: 68 C, calibration data 0x59f4f17d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 11000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [WDOG ]
Boot Device: SPI NOR
I2C: ready
DRAM: 1 GB
NAND: gpmi_reset_block(00112000): module reset timeout
gpmi_reset_block(00112000): module reset timeout
gpmi_reset_block(00112000): module reset timeout
gpmi_reset_block(00112000): module reset timeout
gpmi_reset_block(00112000): module reset timeout
gpmi_reset_block(00112000): module reset timeout
gpmi_reset_block(00112000): module reset timeout
gpmi_reset_block(00112000): module reset timeout
gpmi_reset_block(00112000): module reset timeout
gpmi_reset_block(00112000): module reset timeout
[send_command] DMA error
Command execute failed!
[send_command] DMA error
Command execute failed!
[read_data] DMA error
[read_data] DMA error
[send_command] DMA error
Command execute failed!
[read_data] DMA error
[read_data] DMA error
[send_command] DMA error
Command execute failed!
[read_data] DMA error
[send_command] DMA error
Command execute failed!
[read_data] DMA error
[read_data] DMA error
[read_data] DMA error
[read_data] DMA error
[read_data] DMA error
[read_data] DMA error
[read_data] DMA error
[read_data] DMA error
No NAND device found!!!
0 MiB
JEDEC ID: 0xbf:0x25:0x41
Reading SPI NOR flash 0xc0000 [0x2000 bytes] -> ram 0x27602cc8
SUCCESS

In: serial
Out: serial
Err: serial
Net: got MAC address from IIM: 00:00:00:00:00:00
FEC0 [PRIME]
Hit any key to stop autoboot: 0
MX6Q SABRESD U-Boot >

0 项奖励
回复
0 回复数