imx6q) How to test SPI, UART, CAN ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q) How to test SPI, UART, CAN ?

2,679件の閲覧回数
ktc7270
Contributor II

HI,

I want to test imx6q-sabresd. The device driver seems to be properly configured.

I want to know if there are test codes.

For example, the test code can transfer the spi data of the imx6 board to another board.

(The data received from the imx6 board can do something else through the test code.

Please help me.

ps. add questions.

ラベル(2)
2 返答(返信)

2,084件の閲覧回数
winy2014
Contributor II

Hi,

if users use i.MX6Q board designed by Forlinx, generally the related codes are provided.

Rgds,

Grace

0 件の賞賛

2,083件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kangta

for testing one can use unit tests described in Chapter 9 Unit Tests attached Linux Manual

imx-test
https://source.codeaurora.org/external/imx/imx-test/tree/?h=imx_4.9.88_2.0.0_ga

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------