Hi,
I've an issue while launching Qt5 application on imx6q
Boot Log:
------------
QEglFSVivIntegration will set environment variable FB_MULTI_BUFFER=2 to enable double buffering and vsync.
If this is not desired, you can override this via: export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1
Could not open egl display
I'm using opensource Linux, with following gpu drivers enabled.
drivers/gpu/drm/etnaviv/
drivers/gpu/drm/imx/
Kernel boot log with gpu drivers probe:
[ 1.004653] console [ttymxc3] enabled
[ 1.018428] etnaviv gpu-subsystem: bound 134000.gpu (ops gpu_ops)
[ 1.024690] etnaviv gpu-subsystem: bound 130000.gpu (ops gpu_ops)
[ 1.030855] etnaviv gpu-subsystem: bound 2204000.gpu (ops gpu_ops)
[ 1.037109] etnaviv-gpu 134000.gpu: model: GC320, revision: 5007
[ 1.099266] etnaviv-gpu 130000.gpu: model: GC2000, revision: 5108
[ 1.159483] etnaviv-gpu 2204000.gpu: model: GC355, revision: 1215
[ 1.165658] etnaviv-gpu 2204000.gpu: Ignoring GPU with VG and FE2.0
[ 1.173620] [drm] Initialized etnaviv 1.0.0 20151214 for gpu-subsystem on minor 0
[ 1.183782] imx-ipuv3 2400000.ipu: IPUv3H probed
[ 1.190614] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.197322] [drm] No driver support for vblank timestamp query.
[ 1.203882] imx-drm display-subsystem: bound imx-ipuv3-crtc.2 (ops ipu_crtc_ops)
[ 1.211561] imx-drm display-subsystem: bound imx-ipuv3-crtc.3 (ops ipu_crtc_ops)
[ 1.219193] imx-drm display-subsystem: bound imx-ipuv3-crtc.6 (ops ipu_crtc_ops)
[ 1.226945] imx-drm display-subsystem: bound imx-ipuv3-crtc.7 (ops ipu_crtc_ops)
[ 1.235049] imx-drm display-subsystem: bound 2000000.aips-bus:ldb (ops imx_ldb_ops)
[ 1.320310] Console: switching to colour frame buffer device 160x50
[ 1.344928] imx-drm display-subsystem: fb0: frame buffer device
[ 1.352725] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[ 1.360634] imx-ipuv3 2800000.ipu: IPUv3H probed
[ 1.389001] brd: module loaded
[ 1.412530] loop: module loaded
Please let me know if I miss anything here, the same rootfs with Qt5 is working fine with freesacle kernel.
Thanks.
Hi Jagan
in general for non-nxp kernels issues one can also post on
meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------