imx6q实现lcd和lvds双显

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q实现lcd和lvds双显

1,866 Views
yangzhu
Contributor I

使用IMX6Quad的imx6q-sabresd平台,BSP为L4.1.15-1.0.0的版本,是带QT的linux系统,而不是android。如何实现同时从lcd和lvds输出相同内容?能简单通过boot参数来设置么?有相关的文档参考,或者具体的步骤么?

0 Kudos
3 Replies

1,305 Views
yyuan
Contributor III

你好

我也遇到了相同的问题,用的内核和您的一样,请问您的问题解决了吗?

开机启动的时候  logo只在fb0上显示,不在fb1显示。请问您是怎么解决的呢?

谢谢

0 Kudos

1,305 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi yang,

The linux BSP on imx6q-sabresd do not support dual screen display at the same time. But the android BSP support, and you just need to configure the boot command in u-boot, it can work.

Here you need to output the same on the lcd and LVDS screen, you mean play videos or ...? Could you please describe it in details?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,305 Views
yangzhu
Contributor I

hi,Dan

         firstly,thanks for your help.I want to play video on the LVDS and LCD.If i do that,how to do?

0 Kudos