Hi
I will send a detailed document on how to port audio driver to i.MX6, check your email, please!
Br,
weidong
Hi Yaojun,
你使用的audio code与WM8962的接口非常接近,所以您可以参考开发板上WM8962的驱动编写方法。它比WM8962还要更简单一些。
The audio code you use is very close to the interface of WM8962, so you can refer to the driver writing method of WM8962 on the development board. It's simpler than WM8962.
Have a nice day!
BR,
Weidong
你好,
cs4344芯片因为没有iic或spi的配置引脚,这个芯片只是需要MCLK BCLK LRCLK DATA即可使用,wm8962是iic控制的,所以在dtb中需要添加iic codec的device,在驱动中添加codec driver。
不知道这种情况的芯片在dtb中是否也需要添加codec 的device,类似于 :
sound{
...
audio-codec = <&codec>;
...
}
我想应该没必要?
另外,为了方便调试,我把codec driver和machine driver都放在imx-cs4344.c中编译,这个应该没问题,只是不符合标准。
Wigros Sun, please send me such the document too!
Hi yaojun,
>>Playing WAVE '1k.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
aplay: pcm_write:1947: write error: Invalid argument
Yes, the error should be caused by drivers.
>>no source widget found for playback
no, you can't igore the error. playback path consists of some widgets, the error indicates that the configuration of audio-routing node in device tree is not correct.
You will have to spend some time to understand Linux SoC ALSA driver.
ALSA driver consists of 3 parts:
-platform driver: i.MX6 SSI side, has been supported by BSP
-codec driver: CS4344 side, should be provide by manufacture.
-machine driver: DAI LINK. It is responsible for connetions between CPU DAI and CODEC DAI.
Generally speaking, you should write Machine driver by yourself, for example, you write imx-cs4344.c for you application. Then configure sound card in your device tree to load machine driver.
According to above error messages, they are caused by machine driver and device tree.
Have a nice day!
BR,
Weidong
你好,感谢你的回复,目前我已把声卡驱动成功,但是在aplay的时候出现错误,是否和驱动有关?
root@imx6qsabresd:/home# aplay -Dhw:cs4344 1k.wav
Playing WAVE '1k.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
aplay: pcm_write:1947: write error: Invalid argument