imx6Q ipu video display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6Q ipu video display

992 Views
segri544
Contributor II

Hi Community,

İ am using İMX6Q, i am trying to make 32 MSI interrupt by using 

ret = pci_alloc_irq_vectors(dev, 1, 32, PCI_IRQ_MSI);
 
ret is returned as 16. But i am expecting 32 as documantation (The MSI Driver Guide HOWTO) suggests
"If a device supports both MSI-X and MSI capabilities, this API will use the
MSI-X facilities in preference to the MSI facilities. MSI-X supports any
number of interrupts between 1 and 2048. In contrast, MSI is restricted to
a maximum of 32 interrupts (and must be a power of two)."
 
What could be go wrong? or is max number of MSI is 16?
0 Kudos
Reply
2 Replies

970 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The IPU is binary i can not interrupt or you will have the non-wished results.

Regards

 

0 Kudos
Reply

967 Views
segri544
Contributor II
The title is incorrect; it should be: 'IMX6Q Maximum MSI Signal That Can Be Generated.'
0 Kudos
Reply