For the PAL input, the output is non-standard by tp2825。
it can't lock vsync
refer to the patch https://community.nxp.com/docs/DOC-330441?commentID=41815#comment-41815 ;
experimental result;
how do even field and odd field combine?
Hi,
You can refer to the patch https://community.nxp.com/docs/DOC-330441?commentID=41815#comment-41815 .
Have a nice day
Rita
this is implement by IPU_CSI_CLK_MODE_CCIR656_PROGRESSIVE
the output is Y-C Interleaving output mode per 8-bit. field rate is 50Hz.frame rate is 25hz; pclk is 74.25MHz; resolution is 1920X576;pixelformat = V4L2_PIX_FMT_UYVY;
never-displayed