imx6 ul 9x9 usb otg2 used as device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 ul 9x9 usb otg2 used as device

679 Views
zhougoal
Contributor I

Hello, I use otg1 as host , use otg2 as device, it does not confict with the rule that imx6ul can only have one otg?

But now I cant detect OTG2 as a device, it only respond that a low speed device detected and time out(-32),  what's wrong?

Labels (1)
0 Kudos
2 Replies

554 Views
zhougoal
Contributor I

The problem was solved because our Hardware engineer had turn over the D+ and D-.....

0 Kudos

554 Views
art
NXP Employee
NXP Employee

Of course, you can use USB_OTG1 port as Host only and USB_OTG2 port as Device only. In that case, you have to configure USB_OTG2 port for Device only mode, refer to the Section 4.10 of the attached document for the information on how to do that. Also, check that USB_OTG2_VBUS voltage is present during the Device operation.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos