Hi,
I am working on a custom board with an imx6d processor and a tlv320aic3204 codec.
The codec is connected on the AUD4 port and the mclk comes from GPIO0 at 24MHz.
The codec is detected and the ssi maping seems fine.
imx-aic32x4 sound.18: tlv320aic32x4-hifi <-> 202c000.ssi mapping ok
ALSA device list:
#0: tlv320aic32x4
Here is my device tree entry for the sound card:
sound {
compatible = "fsl,imx-audio-aic32x4";
model = "tlv320aic32x4";
audio-codec = <&codec>;
ssi-controller = <&ssi1>;
audio-routing =
"Line Out Jack", "LOL",
"Line Out Jack, "LOR",
"Headphone Jack, "HPL",
"Headphone Jack, "HPR";
mux-ext-port = <4>;
mux-int-port = <1>;
};
&ssi1 {
status = "okay";
};
... --- ...
codec: tlv320aic32x4@18 {
compatible = "ti,tlv320aic32x4";
reg = <0x18>;
clocks = <&clks 201>;
clock-names = "mclk";
gpio-reset = <&gpio5 12 0>;
status = "okay";
};
When I play with alsamixer, I can see I2C data on the port with the scope.
I don't see data on the AUD4 pins, only the Mclk is always present.
If I use aplay, I get this message after 13s waiting:
aplay: pcm_write:1947: write error: Input/output error
I wrote a machine driver for the tlv320aic32x4 based on the sgtl5000 one...
I use the 3.10.17 kernel on poky-dizzy and the meta-fsl-arm layer in dizzy too.
Regards,
解決済! 解決策の投稿を見る。
I finally managed to fix the issue. Since the driver now supports device tree, a parameter was kept uninitialized... pwr_config.
Just setting pwr_config with a good value solved the issue.
I finally managed to fix the issue. Since the driver now supports device tree, a parameter was kept uninitialized... pwr_config.
Just setting pwr_config with a good value solved the issue.
Hi Benoit,
I face a similar issue with another SoM, but I did not found any "pwr_config" parameter in any driver.
Where does this property come from ?
What does it represent and what value do you use ?
Thank you,
Miquel
Hi Miquel,
It comes from the tlv320aic32x4.c driver. Under the parse_dt function. I
have a patched version of the driver that use device tree, so it is maybe
why you did not see that parameter.
aic32x4->power_cfg
In fact you just have to be sure that your driver enables the internal LDO
of the codec.
snd_soc_write(codec, AIC32X4_LDOCTL, AIC32X4_LDOCTLEN);
Best regards,
Benoit
2016-02-29 8:11 GMT-05:00 kesaco <admin@community.freescale.com>:
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
imx6 - tlv320aic32x4 codec no data on I2S port
reply from Miquèl Raynal
<https://community.freescale.com/people/kesaco?et=watches.email.thread>
in i.MX Community - View the full discussion
<https://community.freescale.com/message/619562?et=watches.email.thread#619562>
Hi, Benoit
can you give me a copy of this driver(for tlv320aic32x4)?
Hi,
To add details to the problem, I put traces in the fsl_ssi driver. I can see that each time I call an aplay or a speaker test the stream is created and the transfer is started. But there is no activity of sdma and ssi in /proc/interrupt...
I am very close... but there is something important missing.
Regards,
Hi Benoit
one can look at linux-imx_3.10.17_1.0.2_ga-imx-tlv320aic23.patch
How to enable TLV320 on IMX6Q?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you very much for your answer
I already have looked at it and it's seems that what I have done so far matches those information.
There is something missing, probably something obvious...
All drivers are loaded, the codec one, the platform one (fsl_ssi) and the machine one (imx-aic32x4) but no data on the I2S port.
Regards,